This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: 66AK2G12: MII of PRU-ICSS (pr0_mii0_rxlink)

Part Number: 66AK2G12


Hi,

we are planing to use PRU-ICSS0 as Ethernet (full-duplex) using MII.

(1) What is the pr0_mii0_rxlink?

Which MII signals should the pr0_mii0_rxlink is connected to?

(2) According to the "TI Pin Mux Tool," when I set PRU-ICSS1_MII as MII0 Real-time industrial Ethernet (full-duplex),

   the pr0_mii0_rxlink is set as below:

●Design Signal Pad Name is PR0_PRU0_GPO8.

●Selected Mode Number is "1" .

●Ball Name is E6 pin.


Then, this is set as "Input pin" accroding to the data manual Table 4-1 Pin Attributes. ←Is this understanding correct?

(3) If I want to use Ethernet PHY that has TXER(MII transmit Error Input),

    which signal should be connected from PRU-ICSS0 as Ethernet (full-duplex) using MII.


Thanks.