Part Number: AM5728
Hi,
I am trying to follow the tutorial on link below to build up a RSE connection with my AM5728 EVM. However, I don't think my network is set up properly. It says in the tutorial that you can find your EVM IP by typing ifconfig. When I do this is the output I see:
root@am57xx-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr A0:F6:FD:BD:A1:A8
inet6 addr: fe80::a2f6:fdff:febd:a1a8/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:1355 errors:0 dropped:45 overruns:0 frame:0
TX packets:34 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:178451 (174.2 KiB) TX bytes:5741 (5.6 KiB)
Interrupt:90
eth1 Link encap:Ethernet HWaddr A0:F6:FD:BD:A1:A9
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:153370 errors:0 dropped:0 overruns:0 frame:0
TX packets:153370 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:10736164 (10.2 MiB) TX bytes:10736164 (10.2 MiB)
Using ethtool eth0 command, I can see that the link is detected. So I used the inet6 address to set up the RSE connection. In Code Composer Studio my Host Name is given set to "FE80::A2F6:FDFF:FEBD:A1A8" and I connect as root with no password. Then I click on Sftp Files->My Root and IDE displays an error message "Operation failed with exception 'java.lang.NullPointerException'" I am also sending the screenshot to illustrate this.
What is the issue here? How can I set the RSE properly?
Thanks for all the help,
M. Talha Uyar
Screenshot: