This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Processors forum

Part Number: AM3352

Hi,

I am using Sitara Processor AM3352BZCZA100 interfaced to DDR and MMC (SD Card) slot in our board, When trying to boot from SD Card the serial message is getting stuck at Starting Kernel. Please find the serial message below.

U-Boot SPL 2014.07 (Sep 19 2020 - 11:36:54)
Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212
Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212

**** U-boot >>> inside file = board/ti/am335x/mux.c, line num = 400, func = enable_board_pin_mux ****
Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212
Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212
reading u-boot.img
reading u-boot.img


U-Boot 2014.07 (Sep 19 2020 - 11:36:54)

I2C: ready
DRAM: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment

Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212
Net: <ethaddr> not set. Validating first E-fuse MAC
Board identification from EEPROM contents: after
Magic numbr : 0xEE3355AA
Board name : A335BNLT
Board version: 000C
Board serial : 2314BBBK0212

**** U-boot >>> inside file = board/ti/am335x/board.c, line num = 711, func = board_eth_init, PHY_MODE = MII ****
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
3992024 bytes read in 256 ms (14.9 MiB/s)
31506 bytes read in 35 ms (878.9 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x3ce9d8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e725000, end 8e72fb11 ... OK

Starting kernel ...

Please revert me back what could be the problem.

With Regards,

Tintu