Hi All,
I would like to ask a question on AMS[2..0] registers.

According to SPRS345d, AMS[2..0] are part of boot configuration pins. But after checking their connection in the schematics, I found that these pins actually connect to NOR (not considering SRAM and NAND here) address lines A0 and A1, as well as DQ15/A-1.
This seems pretty weird. Why the boot configuration pins are not connected to fixed voltage levels? What are the initial statuses of these pins when the DSP is booting? Do they depend on the status of EMIF devices (NAND, for example)?
Thanks,
Zheng