Hello.
Is it possible to get some assistance with the serial flashing process.
I do not see U-boot start up when i connect to the board with picocom.
So Im assuming the board is unflashed.
My attempts with serial flashing result CRC table loading then UBL loading, very slowly, 3 hrs,
and then the program waits for a BEGIN command from the board to ( I assume ) begin
transferring U-boot binary, but the board sends BOOTME instead.
This is becoming very frustrating after having followed all instruction from the wiki.
and for evaluation purposes I cannot justify buying emulator for $1000's to flash the board
I am quite new to this topic and linux, and hope I am trying to load the correct binaries
sft_DM36x_nand.bin and u-boot-dm-365-evm.bin if not
perhaps someone could link me to the correct binaries, or please help with a way forward.
Many thanks
Darren