I have conducted two tests on the USB OTG of 3715 EVM board:
1. After the sysytem boot up, I attached a keypad device to the OTG port, system does not respond to it. The power to the device is off.
2. The keypad device is attached to the OTG port before system boot up. It can recongise the device and the device is working. But if the device is unplugged and then plugged again, system does not respond to it. There is no power to the device.
Can this problem be fixed?
Regards,
Colman