Part Number: AM3352
Hi,
We have a custom board with an AM3352 mounted on it, and a DDR3 chip.
we had fabricated 2 cards,in which one of the card is having an issue with booting , boot process stops when the kernel takes over.
I am booting from the SD card.
The other card is working properly.
Here is our boot log:
U-Boot SPL 2014.07 (Sep 19 2020 - 11:36:54)
What would be the issue with hardware or any memory related issue?
Help would be appreciated.