This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: deserializer is connected to CSI module 1

Part Number: TDA4VM

Hi ,TI

We are debugging the camera application, and we have encountered some problems at present.

We are using the CSI 1 interface to connect to the deserializer which is MAX96712.

And based on the description of CSI in TRM:CSI_RX_IF0 VP0 connection to VISS only. CSI_RX_IF1 VP0 not connected (NC)

In the process of code execution, the following results are obtained after reading CSI register:

CSI_ RX_ IF_ VBUS2APB0_ INFO_ IRQS : 0x0

CSI_ RX_ IF_ VBUS2APB0_ ERROR_ IRQS : 0x0

CSI_ RX_ IF_ VBUS2APB0_ DPHY_ STATUS : 0x222206

CSI_ RX_ IF_ VBUS2APB1_ INFO_ IRQS : 0x20

CSI_ RX_ IF_ VBUS2APB1_ ERROR_ IRQS : 0x0

CSI_ RX_ IF_ VBUS2APB1_ DPHY_ STATUS : 0x333306

1) If CSI_RX_IF1 is not connected to viss, will it affect the current camera application execution?

2) In the current scheme, csi1 interface is connected to deserializer, and what parameters need to be modified?

3) Whether the current CSI register indicates that all four lanes of csi1 are in stop state, and what are the possible reasons.