Hi experts,
I have noticed that the CPSW9G already have the new feature for PTP/TimeSync in new release of V7.1. Is there any ducument for us to test this new feature?
Thanks,
Hutian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
I have noticed that the CPSW9G already have the new feature for PTP/TimeSync in new release of V7.1. Is there any ducument for us to test this new feature?
Thanks,
Hutian
Hi Hutian,
Can you please refer to below and let me if it helps?
Please refer PTP stack section.
Hi Prasad,
Thanks for your reply. Currently i got the "CPTS event lookup errors" as the doc. said:
[MCU2_0] 10.619292 s: CpswCpts_ioctl: Failed to lookup for event: -14
[MCU2_0] 10.619352 s: EnetMod_ioctl: cpsw9g.cpts: Failed to do IOCTL cmd 0x0101030c: -14
[MCU2_0] 10.619396 s: EnetPer_ioctl: cpsw9g: Failed to do IOCTL cmd 0x0101030c: -14
Could you help me to find the place in SDK to change the "MAC port number" to get PTP?
Thanks,
Hutian
Hi Hutian,
Are you connecting both mac port 2 and mac port 3? The errors/warnings you are getting are because of link not available on the port on which PTP server is listening to.
Also are you able to start PTP daemon on Linux PC side and start sync sequence with the TDA as described in the user guide?