Part Number: PROCESSOR-SDK-AM437X
Hello,
I was in trouble.
I want to use USB Ethernet Adapter in AM437x EVB.
Actually, I have no problem USB Ethernet Adapter(w r8152 chipset) under NFS environment(Ethernet boot mode)
But, I am having a problem with it since I changed boot mood from ethernet to NAND.
My problem is that this device is not linked up even if "ifup" command is executed.
I checked several times about kernel image, device driver, cable connection.
But, I think there is no problem.
There is one thing difference between Ethernet boot mode and NAND boot mode. That's the root file system.
When I use NFS, I have used tisdk-rootfs-image. and now, I am using arago-base-tisdk-image under NAND boot mode.
Please could you help me about this issue?
Best Regards,
HC Kim.