Hi,
In our design, the AM4378 processor is interfaced(MII interface) with DP83620SQE/NOPB. I have performed timing calculation(calculation doesn't include delays due to PCB).
As per DP83620SQE/NOPB datasheet, the maximum data valid after RX_CLK clock rising edge is 30ns. The total clock period is 40ns. As per the AM4378 datasheet, the data(RXD[0:3]) is latched at the next rising edge of the RX_CLK. Hence, the setup time available is 40ns-30ns = 10ns. The required setup time of AM4378 is 8ns. The margin available is 2ns. Hence the setup time is passed.
Whether the timing calculation performed is correct?
Thanks
Viswa