This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Serial Device Interface Issue

Other Parts Discussed in Thread: OMAPL138

Hello

I am working on LCDKOMAPl138 and I need to check USB Serial device interface.for that I  am using Starterware code and using CCS studio I imported

Usb_dev_ser code from /home/OMAPL138_StarterWare_1_10_04_01/build/armv5/cgt_ccs/omapl138/lcdkOMAPL138/usb_dev_serial.

Build the project and Debug

My connection on the board is

1.one cable is connected as serial terminal(Connected to USB-Uart port to PC)

2.2nd is connected between USB-OTG port(As a Serial Device) & Host PC

when I run the code and after successfull run I am giving  command "dmesg"  in linux terminal then following log will appear

$ dmesg

==============================================================================================

[156786.599008] usb 1-3: New USB device found, idVendor=1cbe, idProduct=0002, bcdDevice= 1.00
[156786.599009] usb 1-3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[156786.599010] usb 1-3: Product: Virtual COM Port
[156786.599011] usb 1-3: Manufacturer: Texas Instruments
[156786.599011] usb 1-3: SerialNumber: 12345678
[156786.603866] cdc_acm 1-3:1.0: ttyACM0: USB ACM device

=======================================================================

so it means serial device is detected.

After this I am trying to run a simple program which will transfer data to /dev/ttyACM0 but no changes seen nor data is recieved on /dev/ttyACM0 terminal

and my primary requirement is I want to use Baremetal(Starterware) code only. I have tried using SDK Rtos Pdk but i cant use this code.

please guide me regarding this.

Thanks in advance

regards

shubham