Other Parts Discussed in Thread: DP83620
Hi,
We are using AM4378BZDNA100S in the design. Please provide solutions for the following queries regarding IBIS model of AM4378BZDNA100S
1)The IBIS model is showing error when checked with Hyperlynx Visual IBIS editor (Check syntax(Committee parser)). The error pdf is attached.IBIS error.pdf
2) We are simulating for MII interface. As per IBIS, MII interface models are available in model selector 10. In model selector 10, we are having model 69-model 92. How to select the models for the particular pins? Please explain the following terms available in the model
a)FAST/SLOW - IBIS already contains fast,slow,typ case in the model. Why specifically fast/slow is given?
b)IND
c)What does 5%, 10% indicates?
d)BC40D_H_PUPDOFF_5P_!SC1_3P3 -
What does 5P/10P indicates?
What does SC1_3P3 indicates?
What does BC40D_H indicates?
Thanks
Viswa