This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 : MPEG-2 encoder issue

Guru 10255 points

Hi.
I would like to know about MPEG-2 encoder on the following status.
My questions are the reason and the workaround to this issue.

-Issue: MPEG-2 encode has stopped after a few minutes.
-EVM: DM365
-MPEG-2 Encoder: 01.00.00.07
-DVSDK: 2.10.01.18
- Log
 @0x0867a459:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() ret 0 inId 0 outID 1 generated 18764 bytes
 @0x08684168:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() ret 0 inId 1 outID 2 generated 0 bytes
 @0x0868dd5c:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() ret 0 inId 2 outID 3 generated 18764 bytes
 @0x086979df:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() ret 0 inId 0 outID 1 generated 18764 bytes
 @0x0869ed20:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() ret 40965 inId 1 outID 1 generated 18764 bytes
 @0x0869ee0f:[T:0x413ce490] ti.sdo.dmai - [Venc1] VIDENC1_process() failed with error (40965 ext: 0x0)

Regards,
Kanae

 

  • Hi,

    Did you modify anything in DVSDK?

    Are you able to run other encoders?

    Regards,

    Neelakanth

     

  • Hi, Neelakanth.
    Thank you for your concerning with my question.

    Did you modify anything in DVSDK?
    >>> No.
    Are you able to run other encoders?
    >>>No.

    I also would like to make sure about "IMP2VENC_DynamicParams".
    Do you know the actual performance or result of "IMP2VENC_DynamicParams"?
    If you know how it works, please let me know the details.

    Regars,
    Kanae

  • Hi,

    Can you try running other encoders? Demos from the DVSDK should be able to run out of box. If demos are not running out of box then I will ask concerned team to look into it.

    About the dynamic params (IMPEG2VENC_DynamicParams): Some of the params affect the performance. For ex: reset_vIMCOP_every_frame, when set to 1, it will reduce the performance because at start of every encode code will be loaded into HDVICP memory.

  • Hi.
    JPEG encoder is OK, but others were not checked yet.
    reset_vIMCOP_every_frame sets to 0 because when it set to 1, 
    the encoder
     will reduce the performance as you mentioned.
    I hope you will ask concered team to look into this issue.

    Regards,
    Kanae

  • Kanae,

    Sorry for not being clear in my previous answer. Can you run h.264 or mpeg4 encoders? if these application does not work then I will ask concerned team to look into it.

    When reset_vIMCOP_every_frame is set to 1, the performance will get reduced. This reduction is not significant. What is the perormance you are looking for?

    Regards,

    Neelakanth