Other Parts Discussed in Thread: DM3730
I have a customer who plans on using a CCD signal processor from ADI with the DM3730, and is aware that the timing signals (HSYNC, VSYNC, PCLK) will be slightly different when using the AD9895 AFE. But it is his understanding that the DM3730 provides the capability to specify framing intervals, so he's hoping that he won't need any external programmable logic to generate the proper timing. Can anyone verify if he is correct and interfacing to the image sensor via AD9895 is straightforward? Or are there pitfalls thta he should be aware of?
thanks,
pm