Part Number: 66AK2G12
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hi,
We are using two Hwip interrupts with same priority in Arm a15 core.
In SYS/BIOS user guide i read
"Hardware interrupts are preempted by another interrupt unless interrupts are globally disabled or when specific interrupts are individually disabled."
and
"* On some targets, hardware interrupts can be individually enabled and disabled. This is not true on all targets. Also, some targets have controllers that support hardware interrupt prioritization, in which case a Hwi can only be preempted by a higher-priority Hwi."
Even though we are using same priority for both interrupts, it seems like race condition occurs(a global variable used between these two ISRs). So can an interrupt with same prioirty pre-empt the other? If so how can we disable it?