Hi all,
I am working with a DM368 IPNC camera with using K9F1G08U0B PCB0 SamSung Flash memory.
I am using Nandwriter ultility of Appro to flash UBL-UBOOT and diagnostic but after burn successfully our camera cannot start (I could not see any message in terminal).
I guess we did something wrong with nand partitions and entryPoint + ldAddress setting.
I attached nandwriter.c, device_nand.h and 2 flashing logs as below.
Starting DM36x_NANDWriter. Attempting a global erase of NAND:(y/n) y Erasing block 0x0 through 0x3FE. Enter the binary UBL file Name (enter 'none' to skip) : d:\backup\development_tools\ipnc_arm\PrivateTI_IPNC_DM36x2.5\Utils\bin\dm368\ubl_432arm_340ddr_ipnc_dm368_1.1.0.bin Number of blocks needed for header and data: 0x1 Attempting to start write in block number 0x1. Unprotecting blocks 0x1 through 0x1. Erasing block 0x1 through 0x4. Writing header data to Block 0x1, Page 0x0 Writing image data to Block 0x4, Page 0x0 Writing image data to Block 0x4, Page 0x1 Writing image data to Block 0x4, Page 0x2 Writing image data to Block 0x4, Page 0x3 Writing image data to Block 0x4, Page 0x4 Writing image data to Block 0x4, Page 0x5 Writing image data to Block 0x4, Page 0x6 Writing image data to Block 0x4, Page 0x7 Writing image data to Block 0x4, Page 0x8 Writing image data to Block 0x4, Page 0x9 Writing image data to Block 0x4, Page 0xA Protecting the entire NAND flash. Enter the U-boot or application file name (enter 'none' to skip): d:\backup\development_tools\ipnc_arm\PrivateTI_IPNC_DM36x2.5\Utils\bin\dm368\u-boot-1.3.4-dm368_ipnc_1.0.1.bin Enter the U-boot or application entry point (in hex): 0x81080000 Selected entry point is 0x81080000 Enter the U-boot or application load address (in hex): 0x81080000 Number of blocks needed for header and data: 0x2 Attempting to start write in block number 0x8. Unprotecting blocks 0x8 through 0x9. Erasing block 0x8 through 0xC. Writing header data to Block 0x8, Page 0x0 Writing image data to Block 0xB, Page 0x0 Writing image data to Block 0xB, Page 0x1 Writing image data to Block 0xB, Page 0x2 Writing image data to Block 0xB, Page 0x3 Writing image data to Block 0xB, Page 0x4 Writing image data to Block 0xB, Page 0x5 Writing image data to Block 0xB, Page 0x6 Writing image data to Block 0xB, Page 0x7 Writing image data to Block 0xB, Page 0x8 Writing image data to Block 0xB, Page 0x9 Writing image data to Block 0xB, Page 0xA Writing image data to Block 0xB, Page 0xB Writing image data to Block 0xB, Page 0xC Writing image data to Block 0xB, Page 0xD Writing image data to Block 0xB, Page 0xE Writing image data to Block 0xB, Page 0xF Writing image data to Block 0xB, Page 0x10 Writing image data to Block 0xB, Page 0x11 Writing image data to Block 0xB, Page 0x12 Writing image data to Block 0xB, Page 0x13 Writing image data to Block 0xB, Page 0x14 Writing image data to Block 0xB, Page 0x15 Writing image data to Block 0xB, Page 0x16 Writing image data to Block 0xB, Page 0x17 Writing image data to Block 0xB, Page 0x18 Writing image data to Block 0xB, Page 0x19 Writing image data to Block 0xB, Page 0x1A Writing image data to Block 0xB, Page 0x1B Writing image data to Block 0xB, Page 0x1C Writing image data to Block 0xB, Page 0x1D Writing image data to Block 0xB, Page 0x1E Writing image data to Block 0xB, Page 0x1F Writing image data to Block 0xB, Page 0x20 Writing image data to Block 0xB, Page 0x21 Writing image data to Block 0xB, Page 0x22 Writing image data to Block 0xB, Page 0x23 Writing image data to Block 0xB, Page 0x24 Writing image data to Block 0xB, Page 0x25 Writing image data to Block 0xB, Page 0x26 Writing image data to Block 0xB, Page 0x27 Writing image data to Block 0xB, Page 0x28 Writing image data to Block 0xB, Page 0x29 Writing image data to Block 0xB, Page 0x2A Writing image data to Block 0xB, Page 0x2B Writing image data to Block 0xB, Page 0x2C Writing image data to Block 0xB, Page 0x2D Writing image data to Block 0xB, Page 0x2E Writing image data to Block 0xB, Page 0x2F Writing image data to Block 0xB, Page 0x30 Writing image data to Block 0xB, Page 0x31 Writing image data to Block 0xB, Page 0x32 Writing image data to Block 0xB, Page 0x33 Writing image data to Block 0xB, Page 0x34 Writing image data to Block 0xB, Page 0x35 Writing image data to Block 0xB, Page 0x36 Writing image data to Block 0xB, Page 0x37 Writing image data to Block 0xB, Page 0x38 Writing image data to Block 0xB, Page 0x39 Writing image data to Block 0xB, Page 0x3A Writing image data to Block 0xB, Page 0x3B Writing image data to Block 0xB, Page 0x3C Writing image data to Block 0xB, Page 0x3D Writing image data to Block 0xB, Page 0x3E Writing image data to Block 0xB, Page 0x3F Writing image data to Block 0xC, Page 0x0 Writing image data to Block 0xC, Page 0x1 Writing image data to Block 0xC, Page 0x2 Writing image data to Block 0xC, Page 0x3 Writing image data to Block 0xC, Page 0x4 Writing image data to Block 0xC, Page 0x5 Writing image data to Block 0xC, Page 0x6 Writing image data to Block 0xC, Page 0x7 Writing image data to Block 0xC, Page 0x8 Writing image data to Block 0xC, Page 0x9 Writing image data to Block 0xC, Page 0xA Writing image data to Block 0xC, Page 0xB Protecting the entire NAND flash. Erasing block 0x1B through 0x1F. Erasing block 0x300 through 0x3FF. Enter the Diagnostic file name (enter 'none' to skip): d:\backup\development_tools\ipnc_arm\PrivateTI_IPNC_DM36x2.5\Utils\bin\dm368\diagnostic_ipnc_dm368_1.0.0.bin Number of blocks needed for header and data: 0x2 Attempting to start write in block number 0x18. Unprotecting blocks 0x18 through 0x19. Erasing block 0x18 through 0x1C. Writing header data to Block 0x18, Page 0x0 Writing image data to Block 0x1B, Page 0x0 Writing image data to Block 0x1B, Page 0x1 Writing image data to Block 0x1B, Page 0x2 Writing image data to Block 0x1B, Page 0x3 Writing image data to Block 0x1B, Page 0x4 Writing image data to Block 0x1B, Page 0x5 Writing image data to Block 0x1B, Page 0x6 Writing image data to Block 0x1B, Page 0x7 Writing image data to Block 0x1B, Page 0x8 Writing image data to Block 0x1B, Page 0x9 Writing image data to Block 0x1B, Page 0xA Writing image data to Block 0x1B, Page 0xB Writing image data to Block 0x1B, Page 0xC Writing image data to Block 0x1B, Page 0xD Writing image data to Block 0x1B, Page 0xE Writing image data to Block 0x1B, Page 0xF Writing image data to Block 0x1B, Page 0x10 Writing image data to Block 0x1B, Page 0x11 Writing image data to Block 0x1B, Page 0x12 Writing image data to Block 0x1B, Page 0x13 Writing image data to Block 0x1B, Page 0x14 Writing image data to Block 0x1B, Page 0x15 Writing image data to Block 0x1B, Page 0x16 Writing image data to Block 0x1B, Page 0x17 Writing image data to Block 0x1B, Page 0x18 Writing image data to Block 0x1B, Page 0x19 Writing image data to Block 0x1B, Page 0x1A Writing image data to Block 0x1B, Page 0x1B Writing image data to Block 0x1B, Page 0x1C Writing image data to Block 0x1B, Page 0x1D Writing image data to Block 0x1B, Page 0x1E Writing image data to Block 0x1B, Page 0x1F Writing image data to Block 0x1B, Page 0x20 Writing image data to Block 0x1B, Page 0x21 Writing image data to Block 0x1B, Page 0x22 Writing image data to Block 0x1B, Page 0x23 Writing image data to Block 0x1B, Page 0x24 Writing image data to Block 0x1B, Page 0x25 Writing image data to Block 0x1B, Page 0x26 Writing image data to Block 0x1B, Page 0x27 Writing image data to Block 0x1B, Page 0x28 Writing image data to Block 0x1B, Page 0x29 Writing image data to Block 0x1B, Page 0x2A Writing image data to Block 0x1B, Page 0x2B Writing image data to Block 0x1B, Page 0x2C Writing image data to Block 0x1B, Page 0x2D Writing image data to Block 0x1B, Page 0x2E Writing image data to Block 0x1B, Page 0x2F Writing image data to Block 0x1B, Page 0x30 Writing image data to Block 0x1B, Page 0x31 Writing image data to Block 0x1B, Page 0x32 Writing image data to Block 0x1B, Page 0x33 Writing image data to Block 0x1B, Page 0x34 Writing image data to Block 0x1B, Page 0x35 Writing image data to Block 0x1B, Page 0x36 Writing image data to Block 0x1B, Page 0x37 Writing image data to Block 0x1B, Page 0x38 Writing image data to Block 0x1B, Page 0x39 Writing image data to Block 0x1B, Page 0x3A Writing image data to Block 0x1B, Page 0x3B Writing image data to Block 0x1B, Page 0x3C Writing image data to Block 0x1B, Page 0x3D Writing image data to Block 0x1B, Page 0x3E Writing image data to Block 0x1B, Page 0x3F Writing image data to Block 0x1C, Page 0x0 Writing image data to Block 0x1C, Page 0x1 Writing image data to Block 0x1C, Page 0x2 Writing image data to Block 0x1C, Page 0x3 Writing image data to Block 0x1C, Page 0x4 Writing image data to Block 0x1C, Page 0x5 Writing image data to Block 0x1C, Page 0x6 Writing image data to Block 0x1C, Page 0x7 Writing image data to Block 0x1C, Page 0x8 Writing image data to Block 0x1C, Page 0x9 Writing image data to Block 0x1C, Page 0xA Protecting the entire NAND flash. NAND boot preparation was successful!
/* --------------------------------------------------------------------------
FILE : device_nand.h
PROJECT : TI Booting and Flashing Utilities
AUTHOR : Daniel Allred
DESC : Provides device differentiation for the project files. This
file MUST be modified to match the device specifics.
----------------------------------------------------------------------------- */
#ifndef _DEVICE_NAND_H_
#define _DEVICE_NAND_H_
#include "tistdtypes.h"
// Prevent C++ name mangling
#ifdef __cplusplus
extern far "c" {
#endif
/***********************************************************
* Global Macro Declarations *
***********************************************************/
#define DEVICE_NAND_DATA_OFFSET (0x00000000u)
#define DEVICE_NAND_ALE_OFFSET (0x00000008u)
#define DEVICE_NAND_CLE_OFFSET (0x00000010u)
#define DEVICE_NAND_TIMEOUT (10240)
#define DEVICE_NAND_MAX_BYTES_PER_OP (512) // Max Bytes per operation (EMIF IP constrained)
#define DEVICE_NAND_MAX_SPAREBYTES_PER_OP (16) // Max Spare Bytes per operation
#define DEVICE_NAND_MIN_SPAREBYTES_PER_OP (10) // Min Spare Bytes per operation (ECC operation constrained)
#ifdef IPNC_DM365
// Defines which NAND blocks the RBL will search in for a UBL image
#define DEVICE_NAND_RBL_SEARCH_START_BLOCK (1)
#define DEVICE_NAND_RBL_SEARCH_END_BLOCK (3)
// Defines which NAND blocks are valid for writing the APP data
#define DEVICE_NAND_UBL_SEARCH_START_BLOCK (8)
#define DEVICE_NAND_UBL_SEARCH_END_BLOCK (10)
// Defines which NAND blocks are valid for writing the Diagnostic data
#define DEVICE_NAND_DBL_SEARCH_START_BLOCK (32)
#define DEVICE_NAND_DBL_SEARCH_END_BLOCK (34)
#elif defined(IPNC_DM368)
// Defines which NAND blocks the RBL will search in for a UBL image
#define DEVICE_NAND_RBL_SEARCH_START_BLOCK (1)
#define DEVICE_NAND_RBL_SEARCH_END_BLOCK (3)
// Defines which NAND blocks are valid for writing the APP data
#define DEVICE_NAND_UBL_SEARCH_START_BLOCK (8)
#define DEVICE_NAND_UBL_SEARCH_END_BLOCK (10)
// Defines which NAND blocks are valid for writing the Diagnostic data
#define DEVICE_NAND_DBL_SEARCH_START_BLOCK (24)
#define DEVICE_NAND_DBL_SEARCH_END_BLOCK (26)
#else
// Defines which NAND blocks the RBL will search in for a UBL image
#define DEVICE_NAND_RBL_SEARCH_START_BLOCK (1)
#define DEVICE_NAND_RBL_SEARCH_END_BLOCK (24)
// Defines which NAND blocks are valid for writing the APP data
#define DEVICE_NAND_UBL_SEARCH_START_BLOCK (25)
#define DEVICE_NAND_UBL_SEARCH_END_BLOCK (50)
#endif
/******************************************************
* Global Typedef declarations *
******************************************************/
/***********************************************************
* Global Function Declarations *
***********************************************************/
/***********************************************************
* End file *
***********************************************************/
#ifdef __cplusplus
}
#endif
#endif // End _DEVICE_NAND_H_
/* --------------------------------------------------------------------------
FILE : nandwriter.c
PROJECT : TI Booting and Flashing Utilities
AUTHOR : Sandeep Paulraj
DESC : CCS-based utility to flash the DM36x in preparation for
NAND booting
----------------------------------------------------------------------------- */
// C standard I/O library
#include "stdio.h"
// General type include
#include "tistdtypes.h"
// Device specific CSL
#include "device.h"
// This module's header file
#include "nandwriter.h"
// NAND driver include
#include "nand.h"
#include "device_nand.h"
// Misc. utility function include
#include "util.h"
/************************************************************
* Explicit External Declarations *
************************************************************/
extern __FAR__ Uint32 EMIFStart;
extern __FAR__ Uint32 DDRStart;
/************************************************************
* Local Macro Declarations *
************************************************************/
/************************************************************
* Local Typedef Declarations *
************************************************************/
/************************************************************
* Local Function Declarations *
************************************************************/
static Uint32 nandwriter(void);
static Uint32 LOCAL_writeHeaderAndData(NAND_InfoHandle hNandInfo, NANDWRITER_Boot *nandBoot, Uint8 *srcBuf);
/************************************************************
* Global Variable Definitions
************************************************************/
// Global variables for page buffers
static Uint8* gNandTx;
static Uint8* gNandRx;
/************************************************************
* Global Function Definitions *
************************************************************/
void main( void )
{
int status;
// Init memory alloc pointer
UTIL_setCurrMemPtr(0);
#if defined(IPNC_DM365) || defined(IPNC_DM368)
DEVICE_pinmuxControl(2,0xFFFFFFFF,0x00000000); // EMIFA
#endif
// System init
if (DEVICE_init() !=E_PASS)
{
exit();
}
// DEVICE_pinmuxControl( 0, DEVICE_PINMUX_EMIF_MASK, DEVICE_PINMUX_EMIF_EN );
// Execute the NAND flashing
status = nandwriter();
if (status != E_PASS)
{
DEBUG_printString("\n\nNAND flashing failed!\r\n");
}
else
{
DEBUG_printString( "\n\nNAND boot preparation was successful!\r\n" );
}
}
/************************************************************
* Local Function Definitions *
************************************************************/
static Uint32 nandwriter()
{
Uint32 numPagesUBL;
Uint32 numPagesAPP;
NANDWRITER_Boot gNandBoot;
NAND_InfoHandle hNandInfo;
FILE *fPtr;
Uint8 *ublPtr, *appPtr;
Int32 ublFileSize = 0,ublAllocSize = 0, appFileSize = 0,appAllocSize = 0;
Int8 fileName[256];
Int8 answer[24];
Int32 i=0;
DEBUG_printString("Starting DM36x_NANDWriter.\r\n");
// Initialize NAND Flash
hNandInfo = NAND_open((Uint32)&EMIFStart, (Uint8) DEVICE_emifBusWidth() );
if (hNandInfo == NULL)
{
DEBUG_printString( "\tERROR: NAND Initialization failed.\r\n" );
return E_FAIL;
}
#if defined(IPNC_DM365) || defined(IPNC_DM368)
DEBUG_printString("Attempting a global erase of NAND:(y/n)\r\n");
DEBUG_readString(answer);
if(strcmp(answer,"y")==0){
NAND_globalErase(hNandInfo);
}
#endif
// Read the file from host
DEBUG_printString("Enter the binary UBL file Name (enter 'none' to skip) :\r\n");
DEBUG_readString(fileName);
fflush(stdin);
if (strcmp(fileName,"none") != 0)
{
// Open an File from the hard drive
fPtr = fopen(fileName, "rb");
if(fPtr == NULL)
{
DEBUG_printString("\tERROR: File ");
DEBUG_printString(fileName);
DEBUG_printString(" open failed.\r\n");
return E_FAIL;
}
// Read file size
fseek(fPtr,0,SEEK_END);
ublFileSize = ftell(fPtr);
if(ublFileSize == 0)
{
DEBUG_printString("\tERROR: File read failed.. Closing program.\r\n");
fclose (fPtr);
return E_FAIL;
}
numPagesUBL = 0;
while ( (numPagesUBL * hNandInfo->dataBytesPerPage) < ublFileSize )
{
numPagesUBL++;
}
//We want to allocate an even number of pages.
ublAllocSize = numPagesUBL * hNandInfo->dataBytesPerPage;
// Setup pointer in RAM
ublPtr = (Uint8 *) UTIL_allocMem(ublAllocSize);
for (i=0; i<ublAllocSize; i++)
ublPtr[i]=0x00;
fseek(fPtr,0,SEEK_SET);
if (ublFileSize != fread(ublPtr, 1, ublFileSize, fPtr))
{
DEBUG_printString("\tWARNING: File Size mismatch.\r\n");
}
fclose (fPtr);
gNandBoot.magicNum = UBL_MAGIC_SAFE;
gNandBoot.block = DEVICE_NAND_RBL_SEARCH_START_BLOCK;
gNandBoot.page = 0;
gNandBoot.numPage = numPagesUBL;
gNandBoot.entryPoint = 0x0100; // This fixed entry point will work with the UBLs
gNandBoot.ldAddress = 0; // This doesn't matter for the UBL
if (LOCAL_writeHeaderAndData(hNandInfo,&gNandBoot,ublPtr) != E_PASS)
{
printf("\tERROR: Write failed.\r\n");
return E_FAIL;
}
}
// Read the file from host
DEBUG_printString("Enter the U-boot or application file name (enter 'none' to skip):\r\n");
DEBUG_readString(fileName);
fflush(stdin);
if (strcmp(fileName,"none") != 0)
{
// Open an File from the hard drive
fPtr = fopen(fileName, "rb");
if(fPtr == NULL)
{
DEBUG_printString("\tERROR: File ");
DEBUG_printString(fileName);
DEBUG_printString(" open failed.\r\n");
return E_FAIL;
}
// Read file size
fseek(fPtr,0,SEEK_END);
appFileSize = ftell(fPtr);
if(appFileSize == 0)
{
DEBUG_printString("\tERROR: File read failed.. Closing program.\r\n");
fclose (fPtr);
return E_FAIL;
}
numPagesAPP = 0;
while ( (numPagesAPP * hNandInfo->dataBytesPerPage) < (appFileSize) )
{
numPagesAPP++;
}
// We want to allocate an even number of pages.
appAllocSize = numPagesAPP * hNandInfo->dataBytesPerPage;
// Setup pointer in RAM
appPtr = (Uint8 *) UTIL_allocMem(appAllocSize);
fseek(fPtr,0,SEEK_SET);
if (appFileSize != fread(appPtr, 1, appFileSize, fPtr))
{
DEBUG_printString("\tWARNING: File Size mismatch\n");
}
fclose(fPtr);
// Get the entry point and load addresses
DEBUG_printString("Enter the U-boot or application entry point (in hex): \n");
DEBUG_readString(answer);
gNandBoot.entryPoint = strtoul(answer, NULL, 16);
fflush(stdin);
if ( (gNandBoot.entryPoint < DEVICE_DDR2_START_ADDR) || (gNandBoot.entryPoint >= DEVICE_DDR2_END_ADDR) )
{
DEBUG_printString("\tWARNING: Entry point not in acceptable range - using default 0x81080000.\r\n");
gNandBoot.entryPoint = 0x81080000;
}
else
{
DEBUG_printString("Selected entry point is ");
DEBUG_printHexInt(gNandBoot.entryPoint);
DEBUG_printString("\r\n");
}
DEBUG_printString("Enter the U-boot or application load address (in hex): \r\n");
DEBUG_readString(answer);
gNandBoot.ldAddress = strtoul(answer, NULL, 16);
if ( (gNandBoot.ldAddress < DEVICE_DDR2_START_ADDR) || (gNandBoot.ldAddress >= DEVICE_DDR2_END_ADDR) )
{
DEBUG_printString("\tWARNING: Load address not in acceptable range - using default 0x81080000.\r\n");
gNandBoot.ldAddress = 0x81080000;
}
// gNandBoot.magicNum = UBL_MAGIC_SAFE;
gNandBoot.magicNum = UBL_MAGIC_BIN_IMG;
gNandBoot.block = DEVICE_NAND_UBL_SEARCH_START_BLOCK;
gNandBoot.page = 0;
gNandBoot.numPage = numPagesAPP;
if (LOCAL_writeHeaderAndData(hNandInfo, &gNandBoot, appPtr) != E_PASS)
{
DEBUG_printString("\tERROR: Write Failed\n");
return E_FAIL;
}
#if defined(IPNC_DM365) || defined(IPNC_DM368)
if (NAND_eraseBlocks_with_bb_check(hNandInfo,27,5) != E_PASS)
{
DEBUG_printString("Erase failed\n");
return E_FAIL;
}
if (NAND_eraseBlocks_with_bb_check(hNandInfo,hNandInfo->numBlocks-256,256) != E_PASS)
{
DEBUG_printString("Erase failed\n");
return E_FAIL;
}
}
// Read the file from host
DEBUG_printString("Enter the Diagnostic file name (enter 'none' to skip):\r\n");
DEBUG_readString(fileName);
fflush(stdin);
if (strcmp(fileName,"none") != 0)
{
// Open an File from the hard drive
fPtr = fopen(fileName, "rb");
if(fPtr == NULL)
{
DEBUG_printString("\tERROR: File ");
DEBUG_printString(fileName);
DEBUG_printString(" open failed.\r\n");
return E_FAIL;
}
// Read file size
fseek(fPtr,0,SEEK_END);
appFileSize = ftell(fPtr);
if(appFileSize == 0)
{
DEBUG_printString("\tERROR: File read failed.. Closing program.\r\n");
fclose (fPtr);
return E_FAIL;
}
numPagesAPP = 0;
while ( (numPagesAPP * hNandInfo->dataBytesPerPage) < (appFileSize) )
{
numPagesAPP++;
}
// We want to allocate an even number of pages.
appAllocSize = numPagesAPP * hNandInfo->dataBytesPerPage;
// Setup pointer in RAM
appPtr = (Uint8 *) UTIL_allocMem(appAllocSize);
fseek(fPtr,0,SEEK_SET);
if (appFileSize != fread(appPtr, 1, appFileSize, fPtr))
{
DEBUG_printString("\tWARNING: File Size mismatch\n");
}
fclose(fPtr);
// set the entry point and load addresses
gNandBoot.entryPoint =0x81080040;
//set load address
gNandBoot.ldAddress = 0x81080000;
gNandBoot.magicNum = UBL_MAGIC_BIN_IMG;
gNandBoot.block = DEVICE_NAND_DBL_SEARCH_START_BLOCK;
gNandBoot.page = 0;
gNandBoot.numPage = numPagesAPP;
if (LOCAL_writeHeaderAndData(hNandInfo, &gNandBoot, appPtr) != E_PASS)
{
DEBUG_printString("\tERROR: Write Failed\n");
return E_FAIL;
}
#endif
}
return E_PASS;
}
// Generic function to write a UBL or Application header and the associated data
static Uint32 LOCAL_writeHeaderAndData(NAND_InfoHandle hNandInfo, NANDWRITER_Boot *nandBoot, Uint8 *srcBuf)
{
Uint32 endBlockNum;
Uint32 *headerPtr;
Uint32 blockNum;
Uint32 count;
Uint32 countMask;
Uint32 numBlks;
Uint32 pageNum;
Uint32 i;
Uint8 *dataPtr;
gNandTx = (Uint8 *) UTIL_allocMem(NAND_MAX_PAGE_SIZE);
gNandRx = (Uint8 *) UTIL_allocMem(NAND_MAX_PAGE_SIZE);
for (i=0; i<NAND_MAX_PAGE_SIZE; i++)
{
gNandTx[i]=0xff;
gNandRx[i]=0xff;
}
// Get total number of blocks needed
numBlks = 0;
while ( (numBlks * hNandInfo->pagesPerBlock) < (nandBoot->numPage + 1) )
{
numBlks++;
}
DEBUG_printString("Number of blocks needed for header and data: ");
DEBUG_printHexInt(numBlks);
DEBUG_printString("\r\n");
// Check whether writing UBL or APP (based on destination block)
blockNum = nandBoot->block;
if (blockNum == DEVICE_NAND_RBL_SEARCH_START_BLOCK)
{
endBlockNum = DEVICE_NAND_RBL_SEARCH_END_BLOCK;
}
else if (blockNum == DEVICE_NAND_UBL_SEARCH_START_BLOCK)
{
endBlockNum = DEVICE_NAND_UBL_SEARCH_END_BLOCK;
}
#if defined(IPNC_DM365) || defined(IPNC_DM368)
else if (blockNum == DEVICE_NAND_DBL_SEARCH_START_BLOCK)
{
endBlockNum = DEVICE_NAND_DBL_SEARCH_END_BLOCK;
}
#endif
else
{
// Block number is out of range
return E_FAIL;
}
NAND_WRITE_RETRY:
if (blockNum > endBlockNum)
{
return E_FAIL;
}
DEBUG_printString("Attempting to start write in block number ");
DEBUG_printHexInt(blockNum);
DEBUG_printString(".\r\n");
// Unprotect all needed blocks of the Flash
if (NAND_unProtectBlocks(hNandInfo,blockNum,numBlks) != E_PASS)
{
blockNum++;
DEBUG_printString("Unprotect failed.\r\n");
goto NAND_WRITE_RETRY;
}
// Setup header to be written
headerPtr = (Uint32 *) gNandTx;
headerPtr[0] = nandBoot->magicNum; //Magic Number
headerPtr[1] = nandBoot->entryPoint; //Entry Point
headerPtr[2] = nandBoot->numPage; //Number of Pages
#if defined(IPNC_DM365) || defined(IPNC_DM368)
headerPtr[3] = blockNum+3; //Starting Block Number
headerPtr[4] = 0; //Starting Page Number - always start data in page 1 (this header goes in page 0)
#else
headerPtr[3] = blockNum; //Starting Block Number
headerPtr[4] = 1; //Starting Page Number - always start data in page 1 (this header goes in page 0)
#endif
if ( (blockNum>=DEVICE_NAND_RBL_SEARCH_START_BLOCK) && (blockNum <= DEVICE_NAND_RBL_SEARCH_END_BLOCK) )
{
headerPtr[5] = 0; //nandBoot->ldAddress;
}
else if ( (blockNum>=DEVICE_NAND_UBL_SEARCH_START_BLOCK) && (blockNum<=DEVICE_NAND_UBL_SEARCH_END_BLOCK) )
{
headerPtr[5] = nandBoot->ldAddress; //nandBoot->ldAddress;
}
#if defined(IPNC_DM365) || defined(IPNC_DM368)
else if ( (blockNum>=DEVICE_NAND_DBL_SEARCH_START_BLOCK) && (blockNum<=DEVICE_NAND_DBL_SEARCH_END_BLOCK) )
{
headerPtr[5] = nandBoot->ldAddress; //nandBoot->ldAddress;
}
#endif
else
{
// Block number is out of range
return E_FAIL;
}
pageNum = 0;
// Erase the block where the header goes and the data starts
#if defined(IPNC_DM365) || defined(IPNC_DM368)
if (NAND_eraseBlocks(hNandInfo,blockNum,numBlks+3) != E_PASS)
#else
if (NAND_eraseBlocks(hNandInfo,blockNum,numBlks) != E_PASS)
#endif
{
blockNum++;
DEBUG_printString("Erase failed\n");
goto NAND_WRITE_RETRY;
}
DEBUG_printString("Writing header data to Block ");
DEBUG_printHexInt(blockNum);
DEBUG_printString(", Page ");
DEBUG_printHexInt(pageNum);
DEBUG_printString("\r\n");
if (NAND_writePage(hNandInfo, blockNum, pageNum, gNandTx) != E_PASS)
{
blockNum++;
DEBUG_printString("Write failed\n");
NAND_reset(hNandInfo);
goto NAND_WRITE_RETRY;
}
UTIL_waitLoop(200);
// Verify the page just written
if (NAND_verifyPage(hNandInfo, blockNum, pageNum, gNandTx, gNandRx) != E_PASS)
{
DEBUG_printString("Verify failed. Attempting to clear page\n");
NAND_reset(hNandInfo);
NAND_eraseBlocks(hNandInfo,blockNum,numBlks);
blockNum++;
NAND_reset(hNandInfo);
goto NAND_WRITE_RETRY;
}
// Start writing in page 1 of current block (header was in page 0)
count = 1;
#if defined(IPNC_DM365) || defined(IPNC_DM368)
count = 0;
blockNum+=3;
#endif
// The following assumes power of 2 pagesPerBlock - *should* always be valid
countMask = (Uint32) hNandInfo->pagesPerBlock - 1;
dataPtr = srcBuf;
do
{
DEBUG_printString((Uint8 *)"Writing image data to Block ");
DEBUG_printHexInt(blockNum);
DEBUG_printString((Uint8 *)", Page ");
DEBUG_printHexInt(count & countMask);
DEBUG_printString((Uint8 *)"\r\n");
// Write the UBL or APP data on a per page basis
if (NAND_writePage(hNandInfo, blockNum, (count & countMask), dataPtr) != E_PASS)
{
blockNum++;
DEBUG_printString("Write failed\n");
goto NAND_WRITE_RETRY;
}
UTIL_waitLoop(200);
// Verify the page just written
if (NAND_verifyPage(hNandInfo, blockNum, (count & countMask), dataPtr, gNandRx) != E_PASS)
{
DEBUG_printString("Verify failed. Attempting to clear page\n");
NAND_reset(hNandInfo);
NAND_eraseBlocks(hNandInfo,blockNum,numBlks);
blockNum++;
goto NAND_WRITE_RETRY;
}
count++;
dataPtr += hNandInfo->dataBytesPerPage;
if (!(count & countMask))
{
do
{
blockNum++;
}
while (NAND_badBlockCheck(hNandInfo,blockNum) != E_PASS);
}
} while (count <= nandBoot->numPage);
NAND_protectBlocks(hNandInfo);
return E_PASS;
}
/***********************************************************
* End file *
***********************************************************/
/* --------------------------------------------------------------------------
HISTORY
v1.00 - DJA - 02-Nov-2007
Initial release
-------------------------------------------------------------------------- */
please give me a hand to figure out the issue.
Thank you very much!