Other Parts Discussed in Thread: OMAPL138
Hello
I am working lcdkOMAPL138 and my requirement is I want to test USB_dev_msc driver from the starterware PDK for OMAPL138.
Using CCS studio I imported the USB_dev_Msc driver from OMAPL138_StarterWare_1_10_04_01/build/armv5/cgt_ccs/omapl138/lcdkOMAPL138
Connection between PC and LCDKOMAPL138 device is
1.I have connected Uart-USB port to serial terminal for Serial consol.
2.connected USB - OTG port to host PC
when I debug the code following log will come
======================================================================
usb-storage 1-7:1.0: USB Mass Storage device detected
[22940.604075] scsi host4: usb-storage 1-7:1.0
[22941.630393] scsi 4:0:0:0: Direct-Access TI Mass Storage 1.00 PQ: 0 ANSI: 0
[22941.631222] sd 4:0:0:0: [sdb] 32768 512-byte logical blocks: (16.8 MB/16.0 MiB)
[22941.631483] sd 4:0:0:0: Attached scsi generic sg1 type 0
[22941.631541] sd 4:0:0:0: [sdb] Write Protect is off
[22941.631543] sd 4:0:0:0: [sdb] Mode Sense: 03 00 00 00
[22941.631859] sd 4:0:0:0: [sdb] No Caching mode page found
[22941.631868] sd 4:0:0:0: [sdb] Assuming drive cache: write through
[22951.886154] usb 1-7: reset high-speed USB device number 99 using xhci_hcd
[22957.253922] usb 1-7: device descriptor read/64, error -110
[22972.861765] usb 1-7: device descriptor read/64, error -110
[22973.097798] usb 1-7: reset high-speed USB device number 99 using xhci_hcd
[22978.237687] usb 1-7: device descriptor read/64, error -110
============================================================================================================
It is detecting as a mass storage device(Sdb) but it is not showing in file system.
is this correct code or any modification is required please guide me
Thanks in advance
regards
Shubham