Hello,
What does mean the following sentence?
"Wait monitoring is supported for all configurations except for GPMC_CONFIG1_i[19-18] WAITMONITORINGTIME = 0 for write bursts with a clock divider of 1 or 2 (GPMC_CONFIG1_i[1-0] GPMCFCLKDIVIDER field equal to 0 or 1, respectively)."
This is described at 7.1.2.3.8.3.5 in TRM.
In some cases (such as using the fast GPMC clock (100MHz)), doesn't wait function work correctly?
Our expectations are following:
- AD multiplexing 16 bit mode
- While asserted the wait signal from external in both of RD/WR, RD/WR doesn't happen and GPMC_CLK output forever.
Best Regards,
Nomo