This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3MD: OPTFCLKEN_DLL_CLK

Expert 7150 points

Part Number: TDA3MD

Hi Experts,

I have a question about OPTFCLKEN_DLL_CLK below.

The TRM says "Optional functional clock is disabled. DLL_CLK can be gated when EMIF domain performs sleep transition". Does it mean DLL_CLK is being gated only when EMIF domain performs sleep transition? (i.e. DLL_CLK will run even after OPTFCLKEN_DLL_CLK is set to 0 when it is in active state). Or does it mean DLL_CLK is controlled (gating or running) only when EMIF domain performs sleep transition? (i.e. DLL_CLK is always gated after OPTFCLKEN_DLL_CLK is set to 0). 

Best regards,
Ken