Hi,
I try to load mcu firmware using rproc commands at u-boot prompt and debug it in CCS.I can see the imformation in the disassembly window.But how can I know that I have load the firmware correctly and the mcu runs correctly ?
Regards,
HJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I try to load mcu firmware using rproc commands at u-boot prompt and debug it in CCS.I can see the imformation in the disassembly window.But how can I know that I have load the firmware correctly and the mcu runs correctly ?
Regards,
HJ
Hi HJ,
You need to load the correct symbols and then you can also look at the portions of C code running along with the call trace.
Please click Run -> Load -> Load symbols and then load the *.xer5f or *.out of the firmware running.
Are you running some SDK firmware? If yes, I can help you locate the *xer5f or *.out file for the firmware.
Regards,
Karan