Part Number: OMAP-L138
Hi,
I am trying to setup the yocto (thud) build environment for OMAP LI38 custom board. I have referred the below link for setting up the same.
software-dl.ti.com/.../Overview_Building_the_SDK.html
The command which I used to build is as follows
$ cd build
$ . conf/setenv
$ export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf
$ export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu
$ MACHINE=omapl138-lcdk bitbake arago-base-ti-sdk-image
But My build is hanged in parsing reciepes.
I am using Ubuntu 16.04 host PC for the build.
Please let me know the soultion for the build issue.
Thanks & Regards,
Sharmila D