This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: EMMC boot issue

Part Number: AM5728

Hi ,

We have made Custom board with SD card and EMMC  4G.

With TI-SDK provided  Create_sdcard.sh script only doing partitions on both SD card and EMMC.

With SD card Board is booting fine but same steps i followed for EMMC also given error is coming.

Dex---------: board is board_is_am572x_idk

U-Boot SPL 2019.01-g71691c2 (Dec 04 2020 - 17:51:22 +0530)

DRA752-GP ES2.0
Trying to boot from MMC2_2
Loading Environment from FAT... OK
** Partition 1 not valid on device 1 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat_buf: error reading image u-boot.img, err - -1
Loading Environment from FAT... OK
spl: no partition table found
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Please suggest us any debug procedures.

Thanks and Regards,

Kolla Gnanendra