This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB ACCESS ISSUE

Hi all,

Starting kernel ...

Uncompressing Linux................................................................................................................ done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@intel-ubuntu) (gcc version 4.2.4) #1 PREEMPT Thu Feb 24 20:31:49 IST 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM365 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000
PLL0: vencrate_sd: 27000000, ddrrate: 243000000 mmcsdrate: 121500000
PLL1: armrate: 297000000, voicerate: 20482758, vencrate_hd: 74250000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: mem=120M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,13M davinci_enc_mngr.ch0_output=LCD davinci_enc_mngr.ch0_mode=240x320
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 104704KB available (2845K code, 559K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (no cpio magic); looks like an initrd
Freeing initrd memory: 13312K
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
MUX: initialized SPI0_SDI
MUX: initialized SPI0_SDENA0
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
gpio setup of unused Emac pins
MUX: initialized GPIo15
MUX: initialized GPIO14
MUX: initialized GPIO13
MUX: initialized GPIO12
MUX: initialized GPIO11
MUX: initialized GPIO10
MUX: initialized GPIO9
MUX: initialized GPIO8
MUX: initialized GPIO7
MUX: initialized GPIO6
MUX: initialized GPIO5
MUX: initialized GPIO4
MUX: initialized GPIO3
MUX: initialized GPIO2
MUX: initialized GPIO1
MUX: initialized UART1_RXD
MUX: initialized UART1_TXD
DM365 IPIPE initialized in Single Shot mode
ch0 default output "LCD", mode "NTSC"
VPBE Encoder Initialized
<niklcd_encoder_setoutput>
Start of niklcd_encoder_setmode..
</niklcd_encoder_setoutput>
Niklcd Encoder initialized
<niklcd_encoder_enumoutput>
</niklcd_encoder_enumoutput>
<niklcd_encoder_setoutput>
Start of niklcd_encoder_setmode..
</niklcd_encoder_setoutput>
Start of niklcd_encoder_setmode..
Invalid id...
Set output or mode failed, reset to encoder default...
Niklcd Encoder de-initialized
<niklcd_encoder_setoutput>
Start of niklcd_encoder_setmode..
</niklcd_encoder_setoutput>
Niklcd Encoder initialized
<niklcd_encoder_getoutput>
</niklcd_encoder_getoutput>
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
MUX: initialized VOUT_FIELD_G81
Niklcd encoder initialized
dm365_afew_hw_init
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Feb 28 2011 20:16:19 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
davincifb davincifb.0: dm_osd0_fb: 240x320x16@0,0 with framebuffer size 150KB
davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 230KB
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
<niklcd_encoder_getmode>
</niklcd_encoder_getmode>
davincifb davincifb.0: dm_osd1_fb: 240x320x4@0,0 with framebuffer size 150KB
davincifb davincifb.0: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 230KB
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
facedetect major#: 253, minor# 0
facedetect driver registered
imp serializer initialized
davinci_previewer initialized
davinci_resizer initialized
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Linux video capture interface: v2.00
vpfe_init
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe_probe
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9T001
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9P031
TVP514X : nummber of channels = 1
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP514X
Trying to register davinci display video device.
layer=c282d800,layer->video_dev=c282d960
Trying to register davinci display video device.
layer=c282d600,layer->video_dev=c282d760
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
af major#: 250, minor# 0
AF Driver initialized
aew major#: 249, minor# 0
AEW Driver initialized
i2c /dev entries driver
st: Version 20050830, fixed bufsize 32768, s/g segs 256
osst :I: Tape driver with OnStream support version 0.99.4
osst :I: $Id: osst.c,v 1.73 2005/01/01 21:13:34 wriede Exp $
SCSI Media Changer driver v0.25
scsi0 : scsi_debug, version 1.79 [20060604], dev_size_mb=8, opts=0x0
  Vendor: Linux     Model: scsi_debug        Rev: 0004
  Type:   Direct-Access                      ANSI SCSI revision: 05
SCSI device sda: 16384 512-byte hdwr sectors (8 MB)
sda: Write Protect is off
SCSI device sda: drive cache: write back
SCSI device sda: 16384 512-byte hdwr sectors (8 MB)
sda: Write Protect is off
SCSI device sda: drive cache: write back
 sda: unknown partition table
sd 0:0:0:0: Attached scsi disk sda
sd 0:0:0:0: Attached scsi generic sg0 type 0
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
2 NAND chips detected
Bad block table not found for chip 0
Bad block table not found for chip 1
Bad block table not found for chip 0
Bad block table not found for chip 1
Scanning device for bad blocks
Scanning device for bad blocks
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x003c0000 : "bootloader"
0x003c0000-0x00400000 : "params"
0x00400000-0x00800000 : "kernel"
0x00800000-0x20800000 : "filesystem1"
0x20800000-0x80000000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
dm_spi.0: davinci SPI Controller driver at 0xc887e000 (irq = 42) use_dma=0
116x: driver isp116x-hcd, 03 Nov 2005
sl811: driver sl811-hcd, 19 May 2005
usbcore: registered new driver cdc_acm
drivers/usb/class/cdc-acm.c: v0.25:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
usbcore: registered new driver usbtest
musb_hdrc: version 6.0, pio, host, debug=0
MUX: initialized GPIO33
musb_hdrc: USB Host mode controller at c8886000 using PIO, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.18_pro500-davinci_evm-arm_v5t_le musb-hcd
usb usb1: SerialNumber: musb_hdrc
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NIK:in hub_port_status:ret=4
dummy_hcd dummy_hcd: USB Host+Gadget Emulator, driver 02 May 2005
dummy_hcd dummy_hcd: Dummy host controller
dummy_hcd dummy_hcd: new USB bus registered, assigned bus number 2
usb usb2: Product: Dummy host controller
usb usb2: Manufacturer: Linux 2.6.18_pro500-davinci_evm-arm_v5t_le dummy_hcd
usb usb2: SerialNumber: dummy_hcd
usb usb2: configuration #1 chosen from 1 choice
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
mice: PS/2 mouse device common for all mice
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
RAMDISK: Compressed image found at block 0
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
usb 1-1: new high speed USB device using musb_hdrc and address 2
NIK:in hub_port_status:ret=4
usb 1-1: configuration #1 chosen from 1 choice
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 2 ports detected
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
usb 1-1.1: new high speed USB device using musb_hdrc and address 3
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
usb 1-1.1: Product: Mass Storage Device
usb 1-1.1: Manufacturer: JetFlash
usb 1-1.1: SerialNumber: NR669ICL
usb 1-1.1: configuration #1 chosen from 1 choice
scsi1 : SCSI emulation for USB Mass Storage devices
NIK:in hub_port_status:ret=4
NIK:in hub_port_status:ret=4
EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended
VFS: Mounted root (ext2 filesystem).
Freeing init memory: 184K
_______________________________________ SPOD Initilization Started___________________________________________ 
    Meritup_Innovation_pvt_ltd 
    Banglore 
 (v1.00) (Auth:Nikhil Varghese) : Initialization progressing....

    Kernel release : Linux 2.6.18_pro500-davinci_evm-arm_v5t_le
    Kernel version : #1 PREEMPT Thu Feb 24 20:31:49 IST 2011

 Mounting /proc             : [SUCCESS]
 Mounting /sys              : [SUCCESS]
 Mounting /dev              : [SUCCESS]
 Mounting /dev/pts          : [SUCCESS]
 Populating /dev            : [SUCCESS]
 Mounting other filesystems : [SUCCESS]
Setting Paths.... Starting syslogd           : [SUCCESS]

.....SPOD initialization complete.

Please press Enter to activate this console.   Vendor: JetFlash  Model: Transcend 4GB     Rev: 8.07
  Type:   Direct-Access                      ANSI SCSI revision: 02
SCSI device sdb: 7843840 512-byte hdwr sectors (4016 MB)
sdb: Write Protect is off
sdb: assuming drive cache: write through
SCSI device sdb: 7843840 512-byte hdwr sectors (4016 MB)
sdb: Write Protect is off
sdb: assuming drive cache: write through
 sdb:<7>usb-storage: queuecommand called
 sdb1
sd 1:0:0:0: Attached scsi removable disk sdb
sd 1:0:0:0: Attached scsi generic sg1 type 0

 #

i have given all prints above...my dm365 board is detecting USB devices, but i dont know how to access it...

 

pls help how to mount and access the usb device( with instructions)

and how to read and write the usb device

 

thanks in advance