Hello
I have Starter ware PDk for OMAPL138 development board(LCDK) and I am working SPI driver when i imported SPI driver form build directory under ARm5 it seems not working properly
On the serial console I got the following message
==================================================================================
Welcome to StarterWare SPI application.
Here the SPI controller on the SoC communicates with the Fingerprint Sensor present on the LCDK.
Attempting to Reset the Fingerprint Sensor.
ERROR: Fingerprint Sensor Reset Attempt Unsuccessful.
=================================================================================
I have also tried to get clock pulse on CRO but no change.
I need SPI protocol to interface OLed.
What should I need to do for SPI to work?
Thanks in advance
Regards
Shubham