Part Number: DRA829V
Hello TI team,
We have a use case for Jacinto7 whereby we feed two video streams at 800 Mbps (Output clk 400 MHz) and 1500 Mbps (Output clk 89 MHz) to DPHY_RX0 and DPHY_RX1 modules respectively. TRM contains a programming example for CSI_RX_IF module which is pretty helpful but no such example exists for configuration of DPHY MMRs which contain TBIT and PHY isolation configurations mostly and there's not much explanation around that in the TRM (or I am not able to find it). We mean to write a single driver for CSI_RX_IF and DPHY_RX modules. Do we need any DPHY register configuration for our use case?