This thread is related to the following E2E (https://e2e.ti.com/support/processors/f/791/p/961358/3563510#3563510)
Hi experts.
I received two inquires as follows. In the customer's system, USB0 port is supporting OTG function and this port is used for serial communication with USB-Flash or PC. USB1 port is configured as usb-host and communication-module is attached to this port.
1) Regarding USB1 port(Host), when AM3356 enters to Standby mode, would you think VBUS will be disabled ?
2) Regarding USB0 port(OTG), when AM3356 did wakeup from standby mode, AM3356 was not able to recognize USB Flash. How should customer debug this recognition issue? Can I have your advice, please? ( I translated customer's comments, but, I need to check some of points. When I received their feedback. I will update it.)
Best regards,
Miyazaki