This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515: read data from pcm file

Part Number: TMS320C5515

Dear, 

I am fairly new to programming on the TMS. I am trying to read data from a .pcm file using the fopen and freads. The code is this: 

int main( void )
{
	int v,e,tmp1;
	//int index=0 ;
	FILE  *fpv;
	FILE  *fpo;
	char  tempc[2];

	int U[2]={0,0};
	int A[1]={16384};
	int rho[2]={29491, 29491};  //rho=0.9, rho^2

	printf( "\n***Program has Started***\n" );

	fpv = fopen("..\\data\\in.pcm", "rb");
	printf( "reading file opening\n" );
	fpo = fopen("..\\data\\out.pcm", "wb");
	printf( "writing file opening\n" );

	if (fpv == NULL){
	    printf("Can't open input file\n");
	    return 0;
	}
	if (fpo == NULL){
	    printf("Can't open output file\n");
	    return 0;
	}

	fseek(fpv, 0, SEEK_SET);

	tmp1 = fread(tempc, sizeof(char), 2, fpv);
	if(ferror(fpv)){
	    //printf ("Error Reading from in.pcm\n");
	    perror("Error");
	}
	printf("amount of data read %d\n", tmp1);
	printf("first data is %d\n", tempc[0]);

    	/*
    	 * tempc = pointer to a block of memory with a minimum size of sizeof(char)*2 bytes.
    	 * each element read is one byte sizeof(char). 2 elements are read out at a time
    	 * (hence tempc[2], this is in total one data object that is read consisting of 2
    	 * elements each a char wide)
    	 * fread returns the total amount of elements read to tmp1 (which should be 2)
    	 */

	//Begin filtering the data

    fclose(fpv);
    fclose(fpo);

    printf( "\n***Program has Terminated***\n" );
}

I can "open" the files (which are in a map in the project on CCS), and no errors occur. But, whenever doing fread, it returns 0. Even though, there is data in the file (about 32kB). Any ideas why?