Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829,
hello,
In paper 《J721E DRA829/TDA4VM/AM752x Processors Silicon Revision 1.0》5.4.5.4.1.2.5 HSDIVIDER .
Table 5-2185: the HSDIVIDER output clock frequency is given by the equations "HSDIV_CLKOUT = FOUTP / (HSDIV + 1) ";
Figure 5-1019: HSDIV[0~4] input clock is FOUTPOSTDIV,HSDIV[5~9] input clock is FOUTP;
so equations in table 5-2185 don't match description in Figure 5-1019
Example: MAIN_PLL12_HSDIV0_CLKOUT (DDRSS0) , if I used FOUTP as input clock , MAIN_PLL12_HSDIV0_CLKOUT is 934.4MHz,but if I uses FOUTPOSTDIV as input clock , MAIN_PLL12_HSDIV0_CLKOUT is 467.2 MHz. (TDA4VM Evaluation Module, LINUX SDK 7.0.1)
I want to known whether input clock is always FOUTP When calculate HSDIV_CLKOUT in HSDIV[0 ~ 9] ?
thanks