Part Number: TDA4VM
on behalf of a customer:
Hello,
I need to connect ethernet PHY using HISGMII (2.5 SGMII) which IO operating in CML (current mode logic) with TDA4VM embedded switch (LVDS?)
As I understood only TX path need additional 100ohm differential termination.
Q&A:
1.to which J7 voltage domain should I connect "LVDS receiver supply" ?
2. is there need to place additional capacitors on TX/RX signal lines ?
Thanks, Stefan