Part Number: AM4376
Hi,
we are seeing these dmesg lines saying e.g. "gpio gpiochip6: Persistence not supported for GPIO 6" .
Is there a particular configuration in the device tree that is causing this?
I looked through the low-level Linux gpio code and there is a state called PIN_CONFIG_PERSIST_STATE, but I could not see if there is a configuration using this.
Here is a section of dmesg