Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hello,
Please answer following question of OMAPL138 USB0_VBUS.
Datasheet page 81 describes Absolute Maximum Ratings USB0_VBUS is 5.5V maximum. (Up to a maximum of 24 hours.)
Does this mean that 5V can be applied to USB0_VBUS terminal while any power supplies are off ?
Background of this question:
Our customer is using USB0 as device.
At first, OMAPL138 is powered off and USB0 is connected to working host .
So, 5V VBUS voltage form USB connector is applied to USB0_VBUS of OMAPL138.
Customer concern if this situation cause any damege to OMAPL138.
Regards.