Hi,
I use Flash V1.3 to erase EVM Nand flash, but get some error. The message list below and attached file.
-stdout
-omap 3
-com 4
-t 60
-p EVM_MDDR_HYNIX_2G
-2
chip_erase NANDINFO 0
Leaving parameter file:temp_script.txt
@temp_script.txt
Looking for device (omap com4)
Please turn off device, then turn it on again
Awaiting ASIC id
AsicId items 04
AsicId id 01 05 01 36 30 07 07
AsicId secure_mode 13 02 01 00
AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
Searching 2nd for: EVM_MDDR_HYNIX_2G 363007 07 GP
Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_2g.2nd
Entering parameter file:omapflash2nd.txt at line: 15
-pheriphalboot_reopen
Reading board configuration file Targets\Configurations\configuration_evm37xx_hynix_2g.txt
Reading definition file .\targets\definitions\definitions_omap3.txt
-board_config Targets\Configurations\configuration_evm37xx_hynix_2g.txt
Leaving parameter file:omapflash2nd.txt
Sending size of second file (0x00006804 bytes)
Transferring second file to target (0x6804 bytes)
Closing boot connection
Found device (omap com4)
Waiting for 2nd
Reception failed - timeout after 60 s during peripheral boot (waiting for 2nd)
Console program failed, exit code: 2