Hello
I have two PCs with WinXP Pro SP3.
I try to launch AISgen for OMAPL137 and get CLR:80004005 error from Windows on one of them (AISgen closes after the error message).
Enother PC works fine.
Can anybody help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have two PCs with WinXP Pro SP3.
I try to launch AISgen for OMAPL137 and get CLR:80004005 error from Windows on one of them (AISgen closes after the error message).
Enother PC works fine.
Can anybody help me?
Yuriy Kubasov said:I try to launch AISgen for OMAPL137 and get CLR:80004005 error from Windows on one of them (AISgen closes after the error message).
Enother PC works fine.
Not sure what is going on. Can you try to uninstall/reinstall the AISgen on the computer that gave you the error to see if it was just an installation issue?
Problem was in .NET Framework 2.0
I had to reinstall it and now it works fine.