Part Number: AM3356
Hi Experts,
My customer is developing their system with AM3356(Processor SDK version:06_03_00_106). Customer would like to reduce power consumption. Regarding datasheet Table 5-11 Standby-mode, I received some inquiries.
1) DDR is in self-refresh
Customer would like to configure " DDR is in self-refresh " in Standby mode. Does AM335x already support this in Standby mode? How should customer do this configuration. could you elaborate it, please?
2) eMMC
Customer is using eMMC (u-boot). Customer would like to set eMMC to Low Power Mode. Is Linux-SDK supporting this ? if so, could you teach how customer should do this configuration, please?
3) VDD_MPU = 0.95 V (nom), VDD_CORE = 0.95 V (nom) in Datasheet Table 5-11
According to https://e2e.ti.com/support/processors/f/791/p/952286/3542181#3542181 thread, we understood Linux SDK is not able to control PMIC voltage even if AM335x entered standby mode. Customer also confirmed VDD1 always shows 1.1V and VDD2 always shows 0.95V in both Active mode and Standby mode. Customer is asking how much current is consumed for each VDD_MPU/VDD_CORE in standby mode. Could you clarify them, please?
It will be appreciated if you will share Expert's advice/comments on them.
Best regards,
Miyazaki