Hi everybody
I use ti-c6run_0.94.04.05 with the following arago kernel TAG for OMAP L138 EVM BOARD :
- TAG : v2.6.33-rc4_DAVINCIPSP_03.20.00.13 (http://arago-project.org/git/projects/?p=linux-omapl1.git;a=summary)
The c6run-app examples run correctly ;)
I'd like to use a Real-Time Kernel :
- TAG suivant v2.6.33.7-rt29_DAVINCIPSP_03.30.00.01 (http://arago-project.org/git/projects/?p=linux-omapl1.git;a=summary )
With this kernel, cmemk and dsplinkk modules are inserted correctly.
With this kernel the c6run examples runs correctly on ARM side (not a surprise)
But on DSP side, c6run examples can not run and block the system (hardware reboot is needed ...)
Any clue ?
thanks for your help