We are considering to use BeagleBone-AI as a small server platform for certain mil/gov and edge computing customers. We need to boot standard Linux (its default is Debian, which is fine), use standard monitor and USB keyboard for initial hands-on config, and set up SSH so the server can reside in a lab with other servers for long-term access.
Is this possible ? Assuming so, a question comes up about c66x code development: for the time being, we will need to either bypass or disable EVE cores, OpenCL, video codecs, deep learning framework, etc to run and demo some initial c66x C code. Is that do-able ? Can c66x code do simple things like printf() and fopen/fclose() to save files ?
Later we need EVE cores and possibly TIDL. But for now we need to (i) prove to our customers that TI c66x is still relevant and can function in a modern, small server type of environment, and (ii) convince them they don't need to ditch their existing c67x and c66 TI based board production and move to another SoC vendor.
A reply on this would be helpful, thanks.
-Jeff