Other Parts Discussed in Thread: DRA742, DRA752, PMP
Dear TI,
On our new board, we choose BCM89811 for eth phy, the connection mode is RGMII on RGMII0. The dts file we changed as below:
In dra7-evm.dts file, we add below:
&mac {
status = "okay";
#dual_emac;
ti,no-idle;
};
&davinci_mdio{
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rgmii";
dual_emac_res_vlan = <2>;
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "rgmii";
dual_emac_res_vlan = <1>;
};
In dra7.dtsi file, we keep old config as below:
mac: ethernet@48484000 {
compatible = "ti,dra7-cpsw","ti,cpsw";
ti,hwmods = "gmac";
clocks = <&gmac_main_clk>, <&l3init_clkctrl DRA7_GMAC_CLKCTRL 25>;
clock-names = "fck", "cpts";
cpdma_channels = <8>;
ale_entries = <1024>;
bd_ram_size = <0x2000>;
mac_control = <0x20>;
slaves = <2>;
active_slave = <0>;
cpts_clock_mult = <0x784CFE14>;
cpts_clock_shift = <29>;
reg = <0x48484000 0x1000
0x48485200 0x2E00>;
#address-cells = <1>;
#size-cells = <1>;
/*
* Do not allow gating of cpsw clock as workaround
* for errata i877. Keeping internal clock disabled
* causes the device switching characteristics
* to degrade over time and eventually fail to meet
* the data manual delay time/skew specs.
*/
ti,no-idle;
/*
* rx_thresh_pend
* rx_pend
* tx_pend
* misc_pend
*/
interrupts = <GIC_SPI 334 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 335 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 336 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 337 IRQ_TYPE_LEVEL_HIGH>;
ranges;
syscon = <&scm_conf>;
status = "disabled";
davinci_mdio: mdio@48485000 {
compatible = "ti,cpsw-mdio","ti,davinci_mdio";
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "davinci_mdio";
bus_freq = <1000000>;
reg = <0x48485000 0x100>;
};
cpsw_emac0: slave@48480200 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
cpsw_emac1: slave@48480300 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
phy_sel: cpsw-phy-sel@4a002554 {
compatible = "ti,dra7xx-cpsw-phy-sel";
reg= <0x4a002554 0x4>;
reg-names = "gmii-sel";
};
};
But the eth0 can't up as normal. The log as below:
[12-29 14:20:31.128]U-Boot 2014.07 (Dec 28 2020 - 15:28:50)
[12-29 14:20:31.128]
[12-29 14:20:31.128]CPU : DRA752-GP ES2.0
[12-29 14:20:31.129]Board: DRA7xx
[12-29 14:20:31.182]I2C: ready
[12-29 14:20:31.182]DRAM: 1 GiB
[12-29 14:20:31.207]MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
[12-29 14:20:31.222]Card did not respond to voltage select!
[12-29 14:20:31.222]MMC init failed
[12-29 14:20:31.222]Using default environment
[12-29 14:20:31.223]
[12-29 14:20:31.277]serial# not set, setting...
[12-29 14:20:31.288]SF: Detected W25Q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB, mapped at 5c000000
[12-29 14:20:31.303]SF: Warning - Only lower 16MiB accessible, Full access #define CONFIG_SPI_FLASH_BAR
[12-29 14:20:31.303]Net: <ethaddr> not set. Validating first E-fuse MAC
[12-29 14:20:31.325]Phy not found
[12-29 14:20:31.325]cpsw
[12-29 14:20:32.331]Hit any key to stop autoboot: 0
[12-29 14:20:32.331]WARNING: Could not determine device tree to use
[12-29 14:20:32.331]i2c_write: error waiting for addr ACK (status=0x116)
[12-29 14:20:32.337]tps65903x: could not set LDO1 voltage.
[12-29 14:20:32.409]switch to partitions #0, OK
[12-29 14:20:32.409]mmc0 is current device
[12-29 14:20:32.409]i2c_write: error waiting for addr ACK (status=0x116)
[12-29 14:20:32.417]tps65903x: could not set LDO1 voltage.
[12-29 14:20:32.490]SD/MMC found on device 0
[12-29 14:20:32.490]reading uEnv.txt
[12-29 14:20:32.491]172 bytes read in 3 ms (55.7 KiB/s)
[12-29 14:20:32.491]Loaded environment from uEnv.txt
[12-29 14:20:32.497]Importing environment from mmc0 ...
[12-29 14:20:32.740]4411904 bytes read in 237 ms (17.8 MiB/s)
[12-29 14:20:32.797]89723 bytes read in 46 ms (1.9 MiB/s)
[12-29 14:20:32.797]Booting from mmc0 ...
[12-29 14:20:32.797]Kernel image @ 0x82000000 [ 0x000000 - 0x435200 ]
[12-29 14:20:32.808]## Flattened Device Tree blob at 88000000
[12-29 14:20:32.808] Booting using the fdt blob at 0x88000000
[12-29 14:20:32.813] Loading Device Tree to 8ffe7000, end 8ffffe7a ... OK
[12-29 14:20:32.819]
[12-29 14:20:32.819]Starting kernel ...
[12-29 14:20:32.819]
[12-29 14:20:36.138][ 0.000000] Booting Linux on physical CPU 0x0
[12-29 14:20:36.147][ 0.000000] Linux version 4.19.73-00040-g3d03684-dirty (william@ubuntu) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #11 SMP PREEMPT Mon Dec 28 20:44:45 CST 2020
[12-29 14:20:36.160][ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[12-29 14:20:36.171][ 0.000000] CPU: div instructions available: patching division code
[12-29 14:20:36.172][ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[12-29 14:20:36.182][ 0.000000] OF: fdt: Machine model: TI DRA742
[12-29 14:20:36.182][ 0.000000] Memory policy: Data cache writealloc
[12-29 14:20:36.193][ 0.000000] efi: Getting EFI parameters from FDT:
[12-29 14:20:36.193][ 0.000000] efi: UEFI not found.
[12-29 14:20:36.205][ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[12-29 14:20:36.205][ 0.000000] OF: reserved mem: initialized node cmem@40300000, compatible id shared-dma-pool
[12-29 14:20:36.216][ 0.000000] Reserved memory: regions without no-map are not yet supported
[12-29 14:20:36.227][ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[12-29 14:20:36.227][ 0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
[12-29 14:20:36.238][ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[12-29 14:20:36.250][ 0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
[12-29 14:20:36.261][ 0.000000] Reserved memory: regions without no-map are not yet supported
[12-29 14:20:36.261][ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[12-29 14:20:36.272][ 0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
[12-29 14:20:36.283][ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[12-29 14:20:36.294][ 0.000000] OF: reserved mem: initialized node dsp2-memory@9f000000, compatible id shared-dma-pool
[12-29 14:20:36.294][ 0.000000] Reserved memory: regions without no-map are not yet supported
[12-29 14:20:36.306][ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[12-29 14:20:36.317][ 0.000000] OF: reserved mem: initialized node cmem@A9000000, compatible id shared-dma-pool
[12-29 14:20:36.317][ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 64 MiB
[12-29 14:20:36.328][ 0.000000] OF: reserved mem: initialized node gpu-memory@c0000000, compatible id shared-dma-pool
[12-29 14:20:36.339][ 0.000000] cma: Reserved 64 MiB at 0x00000000bbc00000
[12-29 14:20:36.339][ 0.000000] OMAP4: Map 0x00000000bfd00000 to (ptrval) for dram barrier
[12-29 14:20:36.350][ 0.000000] DRA752 ES2.0
[12-29 14:20:36.350][ 0.000000] random: get_random_bytes called from start_kernel+0xb4/0x470 with crng_init=0
[12-29 14:20:36.361][ 0.000000] percpu: Embedded 16 pages/cpu s36492 r8192 d20852 u65536
[12-29 14:20:36.362][ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 251456
[12-29 14:20:36.371][ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=2979582c-02 rw rootwait ip=none mem=1024M cma=64M
[12-29 14:20:36.384][ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[12-29 14:20:36.395][ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[12-29 14:20:36.404][ 0.000000] Memory: 280724K/1012736K available (10240K kernel code, 340K rwdata, 2804K rodata, 2048K init, 269K bss, 420716K reserved, 311296K cma-reserved, 128000K highmem)
[12-29 14:20:36.408][ 0.000000] Virtual kernel memory layout:
[12-29 14:20:36.417][ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[12-29 14:20:36.429][ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[12-29 14:20:36.429][ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[12-29 14:20:36.440][ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[12-29 14:20:36.440][ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[12-29 14:20:36.451][ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[12-29 14:20:36.451][ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (12256 kB)
[12-29 14:20:36.462][ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[12-29 14:20:36.462][ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 341 kB)
[12-29 14:20:36.473][ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 270 kB)
[12-29 14:20:36.473][ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[12-29 14:20:36.484][ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[12-29 14:20:36.485][ 0.000000] Tasks RCU enabled.
[12-29 14:20:36.495][ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[12-29 14:20:36.495][ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[12-29 14:20:36.507][ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (virt).
[12-29 14:20:36.518][ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[12-29 14:20:36.518][ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[12-29 14:20:36.529][ 0.000018] Switching to timer-based delay loop, resolution 162ns
[12-29 14:20:36.540][ 0.000290] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[12-29 14:20:36.541][ 0.000299] OMAP clocksource: 32k_counter at 32768 Hz
[12-29 14:20:36.551][ 0.000728] Console: colour dummy device 80x30
[12-29 14:20:36.552][ 0.000747] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[12-29 14:20:36.563][ 0.000755] This ensures that you still see kernel messages. Please
[12-29 14:20:36.563][ 0.000763] update your kernel commandline.
[12-29 14:20:36.574][ 0.000795] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[12-29 14:20:36.574][ 0.000813] pid_max: default: 32768 minimum: 301
[12-29 14:20:36.585][ 0.000932] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[12-29 14:20:36.596][ 0.000947] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[12-29 14:20:36.596][ 0.001497] CPU: Testing write buffer coherency: ok
[12-29 14:20:36.607][ 0.001535] CPU0: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulnerable
[12-29 14:20:36.608][ 0.001748] /cpus/cpu@0 missing clock-frequency property
[12-29 14:20:36.619][ 0.001768] /cpus/cpu@1 missing clock-frequency property
[12-29 14:20:36.619][ 0.001780] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[12-29 14:20:36.630][ 0.059919] Setting up static identity map for 0x80200000 - 0x80200060
[12-29 14:20:36.630][ 0.079923] rcu: Hierarchical SRCU implementation.
[12-29 14:20:36.641][ 0.100114] EFI services will not be available.
[12-29 14:20:36.641][ 0.119978] smp: Bringing up secondary CPUs ...
[12-29 14:20:36.652][ 0.200310] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[12-29 14:20:36.652][ 0.200316] CPU1: Spectre v2: using ICIALLU workaround
[12-29 14:20:36.663][ 0.200437] smp: Brought up 1 node, 2 CPUs
[12-29 14:20:36.664][ 0.200448] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[12-29 14:20:36.664][ 0.200457] CPU: All CPU(s) started in SVC mode.
[12-29 14:20:36.675][ 0.200941] devtmpfs: initialized
[12-29 14:20:36.675][ 0.217913] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[12-29 14:20:36.686][ 0.218178] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[12-29 14:20:36.699][ 0.218196] futex hash table entries: 512 (order: 3, 32768 bytes)
[12-29 14:20:36.699][ 0.223093] pinctrl core: initialized pinctrl subsystem
[12-29 14:20:36.708][ 0.223622] DMI not present or invalid.
[12-29 14:20:36.708][ 0.223890] NET: Registered protocol family 16
[12-29 14:20:36.719][ 0.225079] DMA: preallocated 256 KiB pool for atomic coherent allocations
[12-29 14:20:36.719][ 0.225979] omap_hwmod: l3_main_2 using broken dt data from ocp
[12-29 14:20:36.732][ 0.413160] cpuidle: using governor ladder
[12-29 14:20:36.732][ 0.413195] cpuidle: using governor menu
[12-29 14:20:36.732][ 0.422972] OMAP GPIO hardware version 0.1
[12-29 14:20:36.742][ 0.446387] No ATAGs?
[12-29 14:20:36.742][ 0.446463] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[12-29 14:20:36.753][ 0.446478] hw-breakpoint: maximum watchpoint size is 8 bytes.
[12-29 14:20:36.753][ 0.446982] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[12-29 14:20:36.765][ 0.446993] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[12-29 14:20:36.765][ 0.447626] OMAP DMA hardware revision 0.0
[12-29 14:20:36.775][ 0.458922] edma 43300000.edma: memcpy is disabled
[12-29 14:20:36.776][ 0.462420] edma 43300000.edma: TI EDMA DMA engine driver
[12-29 14:20:36.787][ 0.469575] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[12-29 14:20:36.799][ 0.471295] evm_3v3: supplied by evm_12v0
[12-29 14:20:36.799][ 0.471596] evm_5v0: supplied by evm_12v0
[12-29 14:20:36.799][ 0.471891] evm_3v6: supplied by evm_5v0
[12-29 14:20:36.809][ 0.474987] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[12-29 14:20:36.809][ 0.475171] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[12-29 14:20:36.820][ 0.475410] omap-iommu 58882000.mmu: 58882000.mmu registered
[12-29 14:20:36.820][ 0.475643] omap-iommu 55082000.mmu: 55082000.mmu registered
[12-29 14:20:36.832][ 0.476004] omap-iommu 41501000.mmu: 41501000.mmu registered
[12-29 14:20:36.832][ 0.476186] omap-iommu 41502000.mmu: 41502000.mmu registered
[12-29 14:20:36.843][ 0.476450] iommu: Adding device 58820000.ipu to group 1
[12-29 14:20:36.843][ 0.476530] iommu: Adding device 55020000.ipu to group 2
[12-29 14:20:36.853][ 0.476660] iommu: Adding device 40800000.dsp to group 0
[12-29 14:20:36.854][ 0.476879] iommu: Adding device 41000000.dsp to group 3
[12-29 14:20:36.865][ 0.477965] SCSI subsystem initialized
[12-29 14:20:36.865][ 0.479190] palmas 0-0058: IRQ missing: skipping irq request
[12-29 14:20:36.876][ 0.500812] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[12-29 14:20:36.876][ 0.502521] SMPS12: supplied by regulator-dummy
[12-29 14:20:36.877][ 0.504203] SMPS3: supplied by regulator-dummy
[12-29 14:20:36.887][ 0.504553] smps3: Bringing 1500000uV into 1350000-1350000uV
[12-29 14:20:36.888][ 0.506639] SMPS45: supplied by regulator-dummy
[12-29 14:20:36.899][ 0.508462] SMPS6: supplied by regulator-dummy
[12-29 14:20:36.899][ 0.510145] SMPS7: supplied by regulator-dummy
[12-29 14:20:36.899][ 0.511996] SMPS8: supplied by regulator-dummy
[12-29 14:20:36.910][ 0.513673] SMPS9: supplied by regulator-dummy
[12-29 14:20:36.910][ 0.514651] LDO1: supplied by regulator-dummy
[12-29 14:20:36.921][ 0.521144] random: fast init done
[12-29 14:20:36.921][ 0.521305] LDO2: supplied by regulator-dummy
[12-29 14:20:36.921][ 0.531154] LDO3: supplied by regulator-dummy
[12-29 14:20:36.932][ 0.541169] LDO4: supplied by regulator-dummy
[12-29 14:20:36.932][ 0.541888] LDO5: supplied by regulator-dummy
[12-29 14:20:36.943][ 0.542610] LDO6: supplied by regulator-dummy
[12-29 14:20:36.944][ 0.543321] LDO7: supplied by regulator-dummy
[12-29 14:20:36.944][ 0.544042] LDO8: supplied by regulator-dummy
[12-29 14:20:36.955][ 0.544765] LDO9: supplied by regulator-dummy
[12-29 14:20:36.955][ 0.551203] LDOLN: supplied by regulator-dummy
[12-29 14:20:36.966][ 0.561222] LDOUSB: supplied by regulator-dummy
[12-29 14:20:36.966][ 0.573670] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[12-29 14:20:36.977][ 0.574167] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[12-29 14:20:36.977][ 0.574566] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 100 kHz
[12-29 14:20:37.450][ 0.574952] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 100 kHz
[12-29 14:20:37.451][ 0.575140] media: Linux media interface: v0.10
[12-29 14:20:37.451][ 0.575179] videodev: Linux video capture interface: v2.00
[12-29 14:20:37.451][ 0.575251] pps_core: LinuxPPS API ver. 1 registered
[12-29 14:20:37.451][ 0.575260] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[12-29 14:20:37.451][ 0.575281] PTP clock support registered
[12-29 14:20:37.451][ 0.575311] EDAC MC: Ver: 3.0.0
[12-29 14:20:37.451][ 0.576094] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[12-29 14:20:37.451][ 0.576347] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[12-29 14:20:37.451][ 0.576816] Advanced Linux Sound Architecture Driver Initialized.
[12-29 14:20:37.451][ 0.577628] clocksource: Switched to clocksource arch_sys_counter
[12-29 14:20:37.451][ 0.585700] NET: Registered protocol family 2
[12-29 14:20:37.451][ 0.586258] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
[12-29 14:20:37.452][ 0.586287] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[12-29 14:20:37.452][ 0.586353] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[12-29 14:20:37.452][ 0.586480] TCP: Hash tables configured (established 8192 bind 8192)
[12-29 14:20:37.452][ 0.586548] UDP hash table entries: 512 (order: 2, 16384 bytes)
[12-29 14:20:37.452][ 0.586582] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[12-29 14:20:37.452][ 0.586711] NET: Registered protocol family 1
[12-29 14:20:37.452][ 0.607151] RPC: Registered named UNIX socket transport module.
[12-29 14:20:37.452][ 0.607162] RPC: Registered udp transport module.
[12-29 14:20:37.452][ 0.607171] RPC: Registered tcp transport module.
[12-29 14:20:37.452][ 0.607179] RPC: Registered tcp NFSv4.1 backchannel transport module.
[12-29 14:20:37.452][ 0.608266] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[12-29 14:20:37.452][ 0.608483] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[12-29 14:20:37.453][ 0.609439] Initialise system trusted keyrings
[12-29 14:20:37.453][ 0.609570] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[12-29 14:20:37.453][ 0.614514] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[12-29 14:20:37.453][ 0.625009] NFS: Registering the id_resolver key type
[12-29 14:20:37.453][ 0.625030] Key type id_resolver registered
[12-29 14:20:37.453][ 0.625039] Key type id_legacy registered
[12-29 14:20:37.453][ 0.625076] ntfs: driver 2.1.32 [Flags: R/O].
[12-29 14:20:37.453][ 0.626638] Key type asymmetric registered
[12-29 14:20:37.453][ 0.626650] Asymmetric key parser 'x509' registered
[12-29 14:20:37.453][ 0.626701] bounce: pool size: 64 pages
[12-29 14:20:37.453][ 0.626740] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[12-29 14:20:37.453][ 0.626750] io scheduler noop registered
[12-29 14:20:37.453][ 0.626760] io scheduler deadline registered
[12-29 14:20:37.454][ 0.626860] io scheduler cfq registered (default)
[12-29 14:20:37.454][ 0.626870] io scheduler mq-deadline registered
[12-29 14:20:37.454][ 0.626880] io scheduler kyber registered
[12-29 14:20:37.454][ 0.629915] forward deserializer init
[12-29 14:20:37.454][ 0.630040] deserializer initialized
[12-29 14:20:37.454][ 0.630119] forward core_status init
[12-29 14:20:37.454][ 0.630239] cstat initialized
[12-29 14:20:37.454][ 0.632832] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[12-29 14:20:37.454][ 0.641512] evm_1v8: supplied by smps9
[12-29 14:20:37.454][ 0.641764] evm_3v3_sw: supplied by sysen1
[12-29 14:20:37.454][ 0.641983] aic_dvdd: supplied by evm_3v3_sw
[12-29 14:20:37.454][ 0.642063] vtt_fixed: supplied by sysen2
[12-29 14:20:37.454][ 0.686938] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[12-29 14:20:37.455][ 0.690508] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 43, base_baud = 3000000) is a 8250
[12-29 14:20:37.455][ 1.810402] console [ttyS0] enabled
[12-29 14:20:37.455][ 1.814807] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 44, base_baud = 3000000) is a 8250
[12-29 14:20:37.455][ 1.824438] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 45, base_baud = 3000000) is a 8250
[12-29 14:20:37.455][ 1.835428] omap_rng 48090000.rng: Random Number Generator ver. 20
[12-29 14:20:37.455][ 1.835764] random: crng init done
[12-29 14:20:37.455][ 1.855059] brd: module loaded
[12-29 14:20:37.455][ 1.864394] loop: module loaded
[12-29 14:20:37.455][ 1.868203] vmemexp device MAJOR num = 244
[12-29 14:20:37.458][ 1.872333] vmemexp class registered
[12-29 14:20:37.458][ 1.876022] /dev/vmemexp device registered
[12-29 14:20:37.458][ 1.880164] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[12-29 14:20:37.458][ 1.910881] m25p80 spi0.0: found w25q256, expected s25fl256s1
[12-29 14:20:37.458][ 1.925852] m25p80 spi0.0: w25q256 (32768 Kbytes)
[12-29 14:20:37.458][ 1.930686] 10 fixed-partitions partitions found on MTD device spi0.0
[12-29 14:20:37.458][ 1.937154] Creating 10 MTD partitions on "spi0.0":
[12-29 14:20:37.458][ 1.942073] 0x000000000000-0x000000020000 : "ubl"
[12-29 14:20:37.458][ 1.947523] 0x000000020000-0x000000070000 : "boot"
[12-29 14:20:37.458][ 1.953045] 0x000000070000-0x000000080000 : "env"
[12-29 14:20:37.458][ 1.958458] 0x000000080000-0x000000090000 : "partition"
[12-29 14:20:37.459][ 1.964377] 0x000000090000-0x0000000b0000 : "dtb"
[12-29 14:20:37.459][ 1.969777] 0x0000000b0000-0x000001000000 : "core0"
[12-29 14:20:37.459][ 1.975351] 0x000001000000-0x0000017e0000 : "app0"
[12-29 14:20:37.459][ 1.980852] 0x0000017e0000-0x000001fc0000 : "app1"
[12-29 14:20:37.459][ 1.986338] 0x000001fc0000-0x000001fe0000 : "config0"
[12-29 14:20:37.459][ 1.992109] 0x000001fe0000-0x000002000000 : "config1"
[12-29 14:20:37.459][ 1.998092] [bcm898xx]---->bcm898xx_init
[12-29 14:20:37.459][ 2.002270] libphy: Fixed MDIO Bus: probed
[12-29 14:20:37.515][ 2.067666] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[12-29 14:20:37.524][ 2.075360] davinci_mdio 48485000.mdio: detected phy mask fffffffd
[12-29 14:20:37.532][ 2.083696] [bcm898xx]---->bcm898xx_match_phy_device
[12-29 14:20:37.533][ 2.088723] [bcm898xx]---->bcm898xx_probe
[12-29 14:20:37.545][ 2.092769] libphy: 48485000.mdio: probed
[12-29 14:20:37.545][ 2.096800] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Broadcom BCM89811
[12-29 14:20:37.556][ 2.106429] cpsw 48484000.ethernet: Detected MACID = 00:35:ff:4e:29:14
[12-29 14:20:37.568][ 2.113047] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[12-29 14:20:37.568][ 2.119451] cpsw 48484000.ethernet: ALE Table size 1024
[12-29 14:20:37.578][ 2.124738] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[12-29 14:20:37.579][ 2.133503] i2c /dev entries driver
[12-29 14:20:37.593][ 2.142175] cpu cpu0: Linked as a consumer to regulator.11
[12-29 14:20:37.594][ 2.147798] cpu cpu0: Linked as a consumer to regulator.34
[12-29 14:20:37.605][ 2.154635] sdhci: Secure Digital Host Controller Interface driver
[12-29 14:20:37.605][ 2.160866] sdhci: Copyright(c) Pierre Ossman
[12-29 14:20:37.617][ 2.166103] sdhci-pltfm: SDHCI platform and OF driver helper
[12-29 14:20:37.629][ 2.172992] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[12-29 14:20:37.629][ 2.181868] sdhci-omap 4809c000.mmc: Got CD GPIO
[12-29 14:20:37.640][ 2.186698] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.33
[12-29 14:20:37.651][ 2.193705] sdhci-omap 4809c000.mmc: 4809c000.mmc supply vqmmc not found, using dummy regulator
[12-29 14:20:37.651][ 2.202540] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.0
[12-29 14:20:37.663][ 2.209348] sdhci-omap 4809c000.mmc: Dropping the link to regulator.0
[12-29 14:20:37.663][ 2.215890] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.3
[12-29 14:20:37.674][ 2.222771] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[12-29 14:20:37.674][ 2.229463] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_3_3v mode
[12-29 14:20:37.683][ 2.236110] sdhci-omap 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[12-29 14:20:37.718][ 2.268817] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA
[12-29 14:20:37.723][ 2.276794] ledtrig-cpu: registered to indicate activity on CPUs
[12-29 14:20:37.738][ 2.288009] NET: Registered protocol family 10
[12-29 14:20:37.738][ 2.293643] Segment Routing with IPv6
[12-29 14:20:37.749][ 2.297420] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[12-29 14:20:37.749][ 2.303902] NET: Registered protocol family 17
[12-29 14:20:37.760][ 2.308658] Key type dns_resolver registered
[12-29 14:20:37.760][ 2.313138] Registering SWP/SWPB emulation handler
[12-29 14:20:37.776][ 2.317999] omap_voltage_late_init: Voltage driver support not added
[12-29 14:20:37.776][ 2.324415] Power Management for TI OMAP4+ devices.
[12-29 14:20:37.776][ 2.330043] Loading compiled-in X.509 certificates
[12-29 14:20:37.799][ 2.349453] mmc0: host does not support reading read-only switch, assuming write-enable
[12-29 14:20:37.819][ 2.367815] mmc0: new high speed SDXC card at address 0007
[12-29 14:20:37.819][ 2.374932] mmcblk0: mmc0:0007 SL64G 58.3 GiB
[12-29 14:20:37.832][ 2.379498] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[12-29 14:20:37.844][ 2.386145] [drm] No driver support for vblank timestamp query.
[12-29 14:20:37.845][ 2.390927] mmcblk0: p1 p2
[12-29 14:20:37.845][ 2.395123] [drm] Initialized vdrm 1.0.0 20191105 for 44000000.ocp:vdrm@0 on minor 0
[12-29 14:20:37.955][ 2.488585] Console: switching to colour frame buffer device 240x67
[12-29 14:20:37.970][ 2.511538] vdrm 44000000.ocp:vdrm@0: fb0: DRM emulated frame buffer device
[12-29 14:20:37.971][ 2.519032] dmm 4e000000.dmm: workaround for errata i878 in use
[12-29 14:20:37.982][ 2.526572] dmm 4e000000.dmm: initialized all PAT entries
[12-29 14:20:37.983][ 2.532877] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 1
[12-29 14:20:37.993][ 2.540867] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
[12-29 14:20:37.993][ 2.546938] hctosys: unable to open rtc device (rtc0)
[12-29 14:20:38.004][ 2.552791] evm_1v8: disabling
[12-29 14:20:38.005][ 2.555864] aic_dvdd: disabling
[12-29 14:20:38.005][ 2.559039] vmmcwl_fixed: disabling
[12-29 14:20:38.005][ 2.562589] ALSA device list:
[12-29 14:20:38.012][ 2.565568] No soundcards found.
[12-29 14:20:41.628][ 6.180933] EXT4-fs (mmcblk0p2): recovery complete
[12-29 14:20:41.636][ 6.189276] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[12-29 14:20:41.646][ 6.197432] VFS: Mounted root (ext4 filesystem) on device 179:2.
[12-29 14:20:41.654][ 6.205939] devtmpfs: mounted
[12-29 14:20:41.655][ 6.210256] Freeing unused kernel memory: 2048K
[12-29 14:20:41.660][ 6.214954] Run /sbin/init as init process
[12-29 14:20:45.602][ 6.531498] systemd[1]: System time before build time, advancing clock.
[12-29 14:20:45.602][ 6.554937] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[12-29 14:20:45.602][ 6.576726] systemd[1]: Detected architecture arm.
[12-29 14:20:45.602]
[12-29 14:20:45.602]Welcome to Arago 2019.09!
[12-29 14:20:45.602]
[12-29 14:20:45.602][ 6.618779] systemd[1]: Set hostname to <dra7xx-evm>.
[12-29 14:20:45.603][ 6.801149] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[12-29 14:20:45.603][ 6.818480] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[12-29 14:20:45.603][ 7.044708] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[12-29 14:20:45.603][ OK ] Started Dispatch Password Requests to Console Directory Watch.
[12-29 14:20:45.603][ 7.087959] systemd[1]: Listening on initctl Compatibility Named Pipe.
[12-29 14:20:45.603][ OK ] Listening on initctl Compatibility Named Pipe.
[12-29 14:20:45.603][ 7.130920] systemd[1]: Created slice system-serial\x2dgetty.slice.
[12-29 14:20:45.603][ OK ] Created slice system-serial\x2dgetty.slice.
[12-29 14:20:45.604][ 7.168775] systemd[1]: Created slice User and Session Slice.
[12-29 14:20:45.604][ OK ] Created slice User and Session Slice.
[12-29 14:20:45.604][ 7.198132] systemd[1]: Listening on Journal Socket (/dev/log).
[12-29 14:20:45.604][ OK ] Listening on Journal Socket (/dev/log).
[12-29 14:20:45.604][ OK ] Listening on Process Core Dump Socket.
[12-29 14:20:45.604][ OK ] Reached target Remote File Systems.
[12-29 14:20:45.604][ OK ] Listening on Network Service Netlink Socket.
[12-29 14:20:45.604][ OK ] Listening on udev Control Socket.
[12-29 14:20:45.604][ OK ] Reached target Swap.
[12-29 14:20:45.605][ OK ] Reached target Slices.
[12-29 14:20:45.605][ OK ] Listening on udev Kernel Socket.
[12-29 14:20:45.605][ OK ] Created slice system-getty.slice.
[12-29 14:20:45.605][ OK ] Started Forward Password Requests to Wall Directory Watch.
[12-29 14:20:45.605][ OK ] Reached target Paths.
[12-29 14:20:45.605][ OK ] Listening on Journal Socket.
[12-29 14:20:45.605] Starting Journal Service...
[12-29 14:20:45.605] Starting Remount Root and Kernel File Systems...
[12-29 14:20:45.605][ 7.671149] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[12-29 14:20:45.605] Mounting Kernel Debug File System...
[12-29 14:20:45.606] Mounting Temporary Directory (/tmp)...
[12-29 14:20:45.606] Starting udev Coldplug all Devices...
[12-29 14:20:45.606] Starting Create list of required st鈥e nodes for the current kernel...
[12-29 14:20:45.606] Mounting POSIX Message Queue File System...
[12-29 14:20:45.606] Starting Load Kernel Modules...
[12-29 14:20:45.606][ OK ] Started Journal Service.
[12-29 14:20:45.606][ OK ] Started Remount Root and Kernel File Systems.
[12-29 14:20:45.606][ OK ] Mounted Kernel Debug File System.
[12-29 14:20:45.606][ OK ] Mounted Temporary Directory (/tmp).
[12-29 14:20:45.607][ OK ] Started Create list of required sta鈥ice nodes for the current kernel.
[12-29 14:20:45.607][ OK ] Mounted POSIX Message Queue File System.
[12-29 14:20:45.607][FAILED] Failed to start Load Kernel Modules.
[12-29 14:20:45.607]See 'systemctl status systemd-modules-load.service' for details.
[12-29 14:20:45.607] Mounting Kernel Configuration File System...
[12-29 14:20:45.607] Starting Apply Kernel Variables...
[12-29 14:20:45.607] Starting Rebuild Hardware Database...
[12-29 14:20:45.607] Starting Create System Users...
[12-29 14:20:45.607] Starting Flush Journal to Persistent Storage...
[12-29 14:20:45.607][ OK ] Mounted Kernel Configuration File System.
[12-29 14:20:45.607][ OK ] Started Apply Kernel Variables.
[12-29 14:20:45.608][ OK ] Started Create System Users.
[12-29 14:20:45.608][ 8.435879] systemd-journald[91]: Received request to flush runtime journal from PID 1
[12-29 14:20:45.608] Starting Create Static Device Nodes in /dev...
[12-29 14:20:45.608][ OK ] Started Flush Journal to Persistent Storage.
[12-29 14:20:45.611][ OK ] Started Create Static Device Nodes in /dev.
[12-29 14:20:45.612][ OK ] Reached target Local File Systems (Pre).
[12-29 14:20:45.616][ OK ] Reached target Containers.
[12-29 14:20:45.617] Mounting /media/ram...
[12-29 14:20:45.617] Mounting /var/volatile...
[12-29 14:20:45.617][ OK ] Mounted /media/ram.
[12-29 14:20:45.617][ OK ] Started udev Coldplug all Devices.
[12-29 14:20:45.617][ OK ] Mounted /var/volatile.
[12-29 14:20:45.617] Starting Load/Save Random Seed...
[12-29 14:20:45.617][ OK ] Reached target Local File Systems.
[12-29 14:20:45.618] Starting Create Volatile Files and Directories...
[12-29 14:20:45.618] Starting Rebuild Journal Catalog...
[12-29 14:20:45.618] Starting Rebuild Dynamic Linker Cache...
[12-29 14:20:45.618][ OK ] Started Load/Save Random Seed.
[12-29 14:20:45.618][ OK ] Started Create Volatile Files and Directories.
[12-29 14:20:45.618] Starting Update UTMP about System Boot/Shutdown...
[12-29 14:20:45.618] Starting Network Time Synchronization...
[12-29 14:20:45.618][ OK ] Started Update UTMP about System Boot/Shutdown.
[12-29 14:20:45.618][ OK ] Started Rebuild Journal Catalog.
[12-29 14:20:45.618][ OK ] Started Network Time Synchronization.
[12-29 14:20:45.619][ OK ] Reached target System Time Synchronized.
[12-29 14:20:50.947][ OK ] Started Rebuild Hardware Database.
[12-29 14:20:50.980] Starting udev Kernel Device Manager...
[12-29 14:20:51.249][ OK ] Started udev Kernel Device Manager.
[12-29 14:20:51.284] Starting Network Service...
[12-29 14:20:51.416][ OK ] Started Network Service.
[12-29 14:20:51.456] Starting Network Name Resolution...
[12-29 14:20:51.639][ 16.189215] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
[12-29 14:20:51.676][ 16.226953] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
[12-29 14:20:51.730][ 16.281035] omap-rproc 58820000.ipu: assigned reserved memory node ipu1-memory@9d000000
[12-29 14:20:51.787][ 16.339996] remoteproc remoteproc0: 58820000.ipu is available
[12-29 14:20:51.807][ 16.357323] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
[12-29 14:20:51.824][ 16.373484] remoteproc remoteproc0: Direct firmware load for dra7-ipu1-fw.xem4 failed with error -2
[12-29 14:20:51.854][ 16.407384] remoteproc remoteproc0: powering up 58820000.ipu
[12-29 14:20:51.885][ 16.436039] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
[12-29 14:20:51.908][ 16.457734] remoteproc remoteproc0: Direct firmware load for dra7-ipu1-fw.xem4 failed with error -2
[12-29 14:20:51.963][ 16.514304] omap-rproc 55020000.ipu: assigned reserved memory node ipu2-memory@95800000
[12-29 14:20:51.987][ 16.539300] remoteproc remoteproc0: request_firmware failed: -2
[12-29 14:20:52.022][ 16.574912] remoteproc remoteproc1: 55020000.ipu is available
[12-29 14:20:52.074][ 16.625209] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
[12-29 14:20:52.116][ 16.665906] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
[12-29 14:20:52.128][ OK ] Started Network Name Resolution.
[12-29 14:20:52.135][ 16.680530] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memory@99000000
[12-29 14:20:52.195][ OK ] Found device /dev/ttyS0.
[12-29 14:20:52.211][ OK ] Reached target Host and Network Name Lookups.[ 16.757420] remoteproc remoteproc2: 40800000.dsp is available
[12-29 14:20:52.211]
[12-29 14:20:52.226][ OK ] Reached target Network.
[12-29 14:20:52.231][ 16.781377] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
[12-29 14:20:52.245][ 16.792467] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
[12-29 14:20:52.253][ 16.802432] omap-rproc 41000000.dsp: assigned reserved memory node dsp2-memory@9f000000
[12-29 14:20:52.275][ 16.827368] remoteproc remoteproc3: 41000000.dsp is available
[12-29 14:20:52.383][ 16.935525] Driver for 1-wire Dallas network protocol.
[12-29 14:20:52.454][ 17.006888] remoteproc remoteproc2: powering up 40800000.dsp
[12-29 14:20:52.466][ 17.016631] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 901596
[12-29 14:20:52.477][ 17.029990] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[12-29 14:20:52.484][ 17.035900] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[12-29 14:20:52.549][ 17.100997] remoteproc remoteproc3: powering up 41000000.dsp
[12-29 14:20:52.556][ 17.106703] remoteproc remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 901596
[12-29 14:20:52.598][ 17.149797] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[12-29 14:20:52.603][ 17.155728] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[12-29 14:20:52.626][ 17.175806] virtio_rpmsg_bus virtio0: rpmsg host is online
[12-29 14:20:52.631][ 17.182440] remoteproc remoteproc2: registered virtio0 (type 7)
[12-29 14:20:52.642][ 17.193299] remoteproc remoteproc2: remote processor 40800000.dsp is now up
[12-29 14:20:52.676][ 17.229150] virtio_rpmsg_bus virtio1: rpmsg host is online
[12-29 14:20:52.684][ 17.237369] remoteproc remoteproc3: registered virtio1 (type 7)
[12-29 14:20:52.695][ 17.247384] remoteproc remoteproc3: remote processor 41000000.dsp is now up
[12-29 14:20:52.729][ 17.282149] remoteproc remoteproc1: powering up 55020000.ipu
[12-29 14:20:52.745][ 17.287711] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode
[12-29 14:20:52.745][ 17.287889] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 8118748
[12-29 14:20:52.754][ 17.305851] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[12-29 14:20:52.794][ 17.346363] virtio_rpmsg_bus virtio2: rpmsg host is online
[12-29 14:20:52.808][ 17.352005] remoteproc remoteproc1: registered virtio2 (type 7)
[12-29 14:20:52.808][ 17.359683] remoteproc remoteproc1: remote processor 55020000.ipu is now up
[12-29 14:20:52.817][ 17.368630] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[12-29 14:20:52.886][ 17.437558] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[12-29 14:20:52.894][ 17.444030] omap-aes 4b500000.aes: will run requests pump with realtime priority
[12-29 14:20:52.917][ 17.469108] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[12-29 14:20:52.925][ 17.475088] omap-aes 4b700000.aes: will run requests pump with realtime priority
[12-29 14:20:52.958][ 17.508063] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d
[12-29 14:20:52.970][ 17.520327] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered.
[12-29 14:20:53.040][ 17.590470] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x50
[12-29 14:20:53.056][ 17.598747] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50
[12-29 14:20:53.056][ 17.606723] virtio_rpmsg_bus virtio1: creating channel rpmsg-proto addr 0x50
[12-29 14:20:54.665][ 19.216557] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[12-29 14:20:54.691][ 19.241487] omap-des 480a5000.des: will run requests pump with realtime priority
[12-29 14:20:54.709][ OK ] Started Rebuild Dynamic Linker Cache.
[12-29 14:20:54.740] Starting Update is Completed...
[12-29 14:20:54.770][ 19.320677] ahci 4a140000.sata: controller can't do 64bit DMA, forcing 32bit
[12-29 14:20:54.807][ 19.360048] net eth0: initializing cpsw version 1.15 (0)
[12-29 14:20:54.814][ 19.367397] libphy: PHY 48485000.mdio:00 not found
[12-29 14:20:54.827][ 19.380212] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1
[12-29 14:20:54.864][ 19.414861] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[12-29 14:20:54.873][ 19.424406] net eth0: phy "48485000.mdio:00" not found on slave 0, err -19
[12-29 14:20:54.909][ 19.458409] ahci 4a140000.sata: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
[12-29 14:20:54.937][ OK ] Started Update is Completed.
[12-29 14:20:54.954][ 19.500907] scsi host0: ahci
[12-29 14:20:54.955][ 19.505562] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 84
[12-29 14:20:54.999][ 19.547679] [bcm89811]phy_id=0xae025022
[12-29 14:20:54.999][ 19.552709] [bcm89811] 0=>write err = 0x0
[12-29 14:20:55.034][ 19.588355] [bcm89811] 1=>write err = 0x0
[12-29 14:20:55.042][ 19.596330] [bcm89811] RDB reg = 0x4000
[12-29 14:20:55.071][ 19.625336] [bcm89811] 2=>write err = 0x0
[12-29 14:20:55.085][ 19.638860] [bcm89811] 3=>write err = 0x0
[12-29 14:20:55.136][ 19.690879] Broadcom BCM89811 48485000.mdio:01: attached PHY driver [Broadcom BCM89811] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
[12-29 14:20:55.193][ 19.743633] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[12-29 14:20:55.335][ 19.887700] ata1: SATA link down (SStatus 0 SControl 300)
[12-29 14:21:02.905][ 19.988798] pvrsrvkm: loading out-of-tree module taints kernel.
[12-29 14:21:02.905][ 20.027561] pvrsrvkm 56000000.gpu: assigned reserved memory node gpu-memory@c0000000
[12-29 14:21:02.906][ 20.099389] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 2
[12-29 14:21:02.906][ 21.966239] NET: Registered protocol family 45
[12-29 14:21:02.906][ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[12-29 14:21:02.906][ OK ] Created slice system-systemd\x2dfsck.slice.
[12-29 14:21:02.906] Starting File System Check on /dev/mmcblk0p1...
[12-29 14:21:02.906][ OK ] Reached target System Initialization.
[12-29 14:21:02.906][ OK ] Listening on D-Bus System Message Bus Socket.
[12-29 14:21:02.906][ OK ] Listening on dropbear.socket.
[12-29 14:21:02.906][ OK ] Started Daily Cleanup of Temporary Directories.
[12-29 14:21:02.907][ OK ] Reached target Timers.
[12-29 14:21:02.907][ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[12-29 14:21:02.907][ OK ] Reached target Sockets.
[12-29 14:21:02.907][ OK ] Reached target Basic System.
[12-29 14:21:02.907] Starting TI IPC Daemon...
[12-29 14:21:02.907] Starting Permit User Sessions...
[12-29 14:21:02.907] Starting Login Service...
[12-29 14:21:02.907] Starting rc.pvr.service...
[12-29 14:21:02.907] Starting Avahi mDNS/DNS-SD Stack...
[12-29 14:21:02.907][ OK ] Started D-Bus System Message Bus.
[12-29 14:21:02.908][ 25.915038] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[12-29 14:21:02.908][ OK ] Started File System Check on /dev/mmcblk0p1.
[12-29 14:21:02.908][ OK ] Started TI IPC Daemon.
[12-29 14:21:02.908][ OK ] Started Permit User Sessions.
[12-29 14:21:02.908][ OK ] Started rc.pvr.service.
[12-29 14:21:02.908] Starting weston.service...
[12-29 14:21:02.908][ OK ] Started Serial Getty on ttyS0.
[12-29 14:21:02.908][ OK ] Started Getty on tty1.
[12-29 14:21:02.908][ OK ] Reached target Login Prompts.
[12-29 14:21:02.909] Starting Synchronize System and HW clocks...
[12-29 14:21:02.909] Mounting /run/media/mmcblk0p1...
[12-29 14:21:02.909][ OK ] Started weston.service.
[12-29 14:21:02.909][FAILED] Failed to start Synchronize System and HW clocks.
[12-29 14:21:02.909][ 26.327995] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[12-29 14:21:02.909]See 'systemctl status sync-clocks.service' for details.
[12-29 14:21:02.909][ OK ] Mounted /run/media/mmcblk0p1.
[12-29 14:21:02.909][ OK ] Started Vsdk Server.
[12-29 14:21:02.909] Starting telnetd.service...
[12-29 14:21:02.910][ OK ] Started Login Service.
[12-29 14:21:02.910][ OK ] Started Avahi mDNS/DNS-SD Stack.
[12-29 14:21:02.910][ OK ] Started telnetd.service.
[12-29 14:21:02.910][ 26.517020] DMA: Module install successful, device major num = 240
[12-29 14:21:02.910][ OK ] Reached target Multi-User System.
[12-29 14:21:02.910][ 26.526066] DRV: Module install successful
[12-29 14:21:02.910] Starting Update UTMP about System Runlevel Changes...
[12-29 14:21:02.910]insmod: ERROR: could not load module ./bin/cmemk.ko: No such file or directory
[12-29 14:21:03.025][ OK ] Started Update UTMP about System Runlevel Cha
[12-29 14:21:03.056] _____ _____ _ _
[12-29 14:21:03.057]| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
[12-29 14:21:03.067]| | _| .'| . | . | | __| _| . | | | -_| _| _|
[12-29 14:21:03.067]|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
[12-29 14:21:03.078] |___| |___|
[12-29 14:21:03.078]
[12-29 14:21:03.079]Arago Project http://arago-project.org dra7xx-evm ttyS0
[12-29 14:21:03.079]
[12-29 14:21:03.079]Arago 2019.09 dra7xx-evm ttyS0
It looks the connection of phy is ok, the phy register can be read out, but "eth0: Link is Up " not found.
use ifconfig,
[12-29 14:22:28.338]root@dra7xx-evm:/usr# ifconfig
[12-29 14:22:28.372]eth0 Link encap:Ethernet HWaddr 00:35:FF:4E:29:14
[12-29 14:22:28.372] UP BROADCAST MULTICAST MTU:1500 Metric:1
[12-29 14:22:28.384] RX packets:0 errors:0 dropped:0 overruns:0 frame:0
[12-29 14:22:28.384] TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
[12-29 14:22:28.394] collisions:0 txqueuelen:1000
[12-29 14:22:28.394] RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
[12-29 14:22:28.395] Interrupt:87
[12-29 14:22:28.395]
[12-29 14:22:28.404]lo Link encap:Local Loopback
[12-29 14:22:28.405] inet addr:127.0.0.1 Mask:255.0.0.0
[12-29 14:22:28.405] inet6 addr: ::1/128 Scope:Host
[12-29 14:22:28.417] UP LOOPBACK RUNNING MTU:65536 Metric:1
[12-29 14:22:28.418] RX packets:80 errors:0 dropped:0 overruns:0 frame:0
[12-29 14:22:28.428] TX packets:80 errors:0 dropped:0 overruns:0 carrier:0
[12-29 14:22:28.428] collisions:0 txqueuelen:1000
[12-29 14:22:28.428] RX bytes:6080 (5.9 KiB) TX bytes:6080 (5.9 KiB)
use ethtool,
[12-29 14:22:35.130]root@dra7xx-evm:/usr# ./ethtool eth0
[12-29 14:22:35.165]Settings for eth0:
[12-29 14:22:35.166] Supports Wake-on: d
[12-29 14:22:35.166] Wake-on: d
[12-29 14:22:35.166] Current message level: 0x00000000 (0)
[12-29 14:22:35.166]
[12-29 14:22:35.166] Link detected: no
wx.