Part Number: PROCESSOR-SDK-DRA7X
Other Parts Discussed in Thread: DRA722
Hello,
I am using,
CPU : DRA722-GP ES2.0
Model: TI DRA722 Rev C EVM
Board: DRA72x EVM REV C.1
DRAM: 2 GiB
Linux version 4.4.117
Android: Android™ Oreo™ MR1 8.1 (OPM1.171019.021)
Toolchain: Android linux-x86 toolchain android-eabi-4.9
Issue description:
If no LCD display is connected to the board it doesn't boot. If the 10.1" LCD/Touch screen display is attached it boots up successfully.