Part Number: AM5728
Hello,
I am using TI's AM5728 EVM with Android PSDK 5.03 on it.
I would like to add support for Fingerprint (Biometric) Authentication inside Settings application. Currently, there is Security & location tab in Settings application which contains following options for Screen lock under Device security header -
Swipe Pattern PIN Password None
I would like to add Fingerprint option here. This will allow user to Add/Delete fingerprints and also choose it as a Screen Lock option.
I have a Fingerprint device with me which I was able to port for TI's Linux PSDK 6.03. And now I would like to port it for Android PSDK 5.03.
Is it possible ?
Regards,
Devashish