This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL1-38 timer

Other Parts Discussed in Thread: OMAPL138

Hello

 I am shubham,

I am working on LCDK-OMAPL138  board and i am using starter-ware package.

i have imported timer driver available for LCDK-OMAPl138.this code will work fine with 1sec delay but i want to interface 1-wire protocol functionality for that i need delay in micro-seconds

so how to provide time period in micro seconds.using time period register.

i have attached timercounter.c program with this query.

/**
 * \file  timerCounter.c
 *
 * \brief Sample application for timer.
 */

/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ 
*
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/

#include "uart.h"
#include "hw_uart.h"
#include "interrupt.h"
#include "soc_OMAPL138.h"
#include "hw_syscfg0_OMAPL138.h"
#include "timer.h"
#include "lcdkOMAPL138.h"
#include "uartStdio.h"

#ifndef _TMS320C6X
#include "cpu.h"
#endif

/******************************************************************************
**                      INTERNAL MACRO DEFINITIONS
*******************************************************************************/
#define STR_LEN                        (13)
#define TMR_PERIOD_LSB32              (0x07FFFFFF)
#define TMR_PERIOD_MSB32               (0x0)

/******************************************************************************
**                      INTERNAL FUNCTION PROTOTYPES
*******************************************************************************/
static void TimerIsr(void);
static void TimerSetUp64Bit(void);
static void TimerIntrSetUp(void);

/******************************************************************************
**                      INTERNAL VARIABLE DEFINITIONS
*******************************************************************************/
static unsigned char cntArr[9] = {'8', '7', '6', '5', '4', '3', '2', '1', '0'};
static volatile unsigned int secCnt = 0;
static volatile unsigned int flagIsrCnt = 0;
static volatile unsigned int SET_FLAG = 0, count = 0;


/******************************************************************************
**                          FUNCTION DEFINITIONS
*******************************************************************************/
int main(void)
    {
    int value = 0;
    /* Set up the UART2 peripheral */
    UARTStdioInit();

    /* Set up the Timer2 peripheral */
    TimerSetUp64Bit();

    /* Set up the AINTC to generate Timer2 interrupts */
    TimerIntrSetUp();

    /* Enable the timer interrupt */
    TimerIntEnable(SOC_TMR_2_REGS, TMR_INT_TMR12_NON_CAPT_MODE);

#ifndef _TMS320C6X
    /* Switch to non privileged mode; This is done for demonstration purpose */
    CPUSwitchToUserMode();
#endif

    /* Send the first String */
    UARTPuts("Tencounter: 9", -1);

    /* Start the timer. Characters from cntArr will be sent from the ISR */
    TimerEnable(SOC_TMR_2_REGS, TMR_TIMER12, TMR_ENABLE_CONT);

    while (1)
    {
#if 0
        /* make sure all the characters from cntArray from ISR */
        while (secCnt < 9)
        {
            /* Replace previous number each time the timer interrupt occurs */
            if (flagIsrCnt)
            {
                UARTPutc('\b');
                UARTPutc(cntArr[secCnt]);
                secCnt++;
                flagIsrCnt = 0;
            }
        }
#endif
        if (SET_FLAG == 1)
        {
            UARTPutNum(value++);
            //UARTPuts("One Second Timer\n", 17);
            SET_FLAG = 0;
            //UARTPutc(secCnt);
            //secCnt++;

        }
        //secCnt = 0;
    }
    /* Disable the timer. No more timer interrupts */
    TimerDisable(SOC_TMR_2_REGS, TMR_TIMER12);

    /* Halt the program */

}

/*
** Timer Interrupt Service Routine
*/
static void TimerIsr(void)
{

    /* Disable the timer interrupt */
    TimerIntDisable(SOC_TMR_2_REGS, TMR_INT_TMR12_NON_CAPT_MODE);

#ifdef _TMS320C6X
    /* Clear interrupt status in DSPINTC */
    IntEventClear(SYS_INT_T64P2_TINTALL);
#else
    /* Clear the interrupt status in AINTC */
    IntSystemStatusClear(SYS_INT_TIMR2_ALL);
#endif
    TimerIntStatusClear(SOC_TMR_2_REGS, TMR_INT_TMR12_NON_CAPT_MODE);

    /* Signal application to print a new character */
    flagIsrCnt = 1;
  
    /* Enable the timer interrupt */
    TimerIntEnable(SOC_TMR_2_REGS, TMR_INT_TMR12_NON_CAPT_MODE);

    count++;

    if (count == (1000*500))
    {
        SET_FLAG = 1;
        count = 0;
    }
}


/*
** Setup the timer for 64 bit mode
*/
static void TimerSetUp64Bit(void)
{
    /* Configuration of Timer */
    TimerConfigure(SOC_TMR_2_REGS, TMR_CFG_64BIT_CLK_INT);

    /* Set the 64 bit timer period */
    TimerPeriodSet(SOC_TMR_2_REGS, TMR_TIMER12, TMR_PERIOD_LSB32);
    TimerPeriodSet(SOC_TMR_2_REGS, TMR_TIMER34, TMR_PERIOD_MSB32);
}

/*
** Set up the ARM Interrupt Controller for generating timer interrupt
*/
static void TimerIntrSetUp(void)
{
#ifdef _TMS320C6X
    /* Initialize the DSPINTC */
    IntDSPINTCInit();

    /* Register the Timer ISR */
    IntRegister(C674X_MASK_INT4, TimerIsr);

    /* Map Timer interrupts to DSP maskable interrupt */
    IntEventMap(C674X_MASK_INT4, SYS_INT_T64P2_TINTALL);

    /* Enable DSP interrupt in DSPINTC */
    IntEnable(C674X_MASK_INT4);

    /* Enable DSP interrupts */
    IntGlobalEnable();
#else
    /* Initialize AINTC and register timer interrupt */
    IntAINTCInit();
    
    /* Register the Timer ISR */
    IntRegister(SYS_INT_TIMR2_ALL, TimerIsr);
  
    /* Set the channel number for Timer interrupt, it will map to IRQ */
    IntChannelSet(SYS_INT_TIMR2_ALL, 2);
   
    /* Enable IRQ for ARM (in CPSR)*/
    IntMasterIRQEnable();
  
    /* Enable AINTC interrupts in GER */
    IntGlobalEnable();

    /* Enable IRQ in AINTC */
    IntIRQEnable();

    /* Enable timer interrupts in AINTC */
    IntSystemEnable(SYS_INT_TIMR2_ALL);
#endif
}
/***************************** End Of File ***********************************/

If you have any suggestion please guide me.

thanks in advance

regards

shubham

  • Hi Shubham

    If you have processor sdk for OMAPL138, it supports the OSAL layer which has the delay in micro seconds.

    Regarding your c file that you provided,

    I see below in your timer ISR:

    count++;

    if (count == (1000*500))
    {
    SET_FLAG = 1;
    count = 0;
    }

    From the code you shared, it appears like 500000 timer ticks map to 1 second.  Can you try to compare the count value to 500 and then SET_FLAG to 1, to measure a milli second duration?

    Wondering if you are facing any issue in that?

    Thanks.

  • Hi Shubham,

    Note that if you do not respond for long (like a month or so), the thread automatically gets locked. I just unlocked it - I will wait for couple of days and if I do not hear back from you, I would assume that there is no further questions on this and I will close the thread after that.

    Thanks

  • Hi Shubham,

    Assuming there is nothing further to discuss on this, closing the thread.

    Thanks