This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 timer1 interrupt refuses to work



 

Hi:

i am trying to generate a square wave from GPIO pin of a C6747, by alternatively setting and clearing the corresponding bit of certain GPIO register in the isr function of timer1 interrupt. the timer1 intterupt works well, but when i add some other lines in my codes, like those marked in red color below, the isr function refuses to execute, although i think they have nothing related with timer1. i checked the core registers of C6747, and also timer1 registers, found nothing unusual, expect that IRP had changed. could someone help me? thanks a lot!

void Timer1_Init(void)
{
    TIMER1_TCR   = 0x00000080; //timer1 control register
    TIMER1_PRD12 = 0x00000330;
    TIMER1_TIM12 = 0;
    INTCTLSTAT1 &= ~0xFF;
    INTCTLSTAT1 |= 0x00000001;   // enable timer1 interrupt
    TIMER1_TGCR  = 0x05;         // let timer1 works in dual 32bit unchained mode and enable time1
}
Uint8 cnt = 0;
void main(void)
{  
    C6747_init( );
    KICK0R = 0x83e70b13;  // Kick0 register + data (unlock)  */
    KICK1R = 0x95a4f1e0;  // Kick1 register + data (unlock)  */
    PINMUX13 = 0x00000080;  //GP4[4]                            */
    KICK0R = 0;  // Kick0 register + data (unlock)           */
    KICK1R = 0;  // Kick1 register + data (unlock)           */
 //   C6747_GPIO_setDirection(4 << 5 + 4, 0); 

    ISTP = 0x80003800;  //start of the c_int0

 
    INTMUX1 &= ~0xFF;   // clear out INTSEL4 field
    INTMUX1 |= 40;      // INTSEL4=40
    IER |= 0x00000013;   // IE4=1
   CSR |= 0x00000001;   // intrrupt gloabe enabel
   Timer1_Init();

 while(1);

}

interrupt void Timer1_isr(void){
// if((cnt++) % 2)                                    
//  GPIO_OUT_DATA45 |= 0x00000010;                   
// else                                                 
//   GPIO_SET_DATA45 &= ~(0x00000010);           
 printf("interrupt occured\n");
          
}