Other Parts Discussed in Thread: SYSBIOS
Hi,
How many timers that can be use in sys/bios?
Customer create a simple project with timer64. When calling Timer_getNumTimers, it returns 16 available timers. But check all timers through Timer_getStatus, only timer id 2 and 3 is FREE, and the other timers are INUSE.
Adding below configuration in .cfg, it still prompts error.
ti_sysbios_timers_timer64_Timer.defaultHalf = ti_sysbios_timers_timer64_Timer.Half_DEFAULT;
ti_sysbios_timers_timer64_Timer.timerSettings[4].ownerCoreId = 0;
Clock.timerId = 4;
Description Resource Path Location Type
ti.sysbios.timers.timer64.Timer.Instance#0 : Timer 4 is already in use or reserved (check availMask/availMaskHigh)。
And i also test with clock demo in sys/bios. Only timerID 0-3 are available.