Other Parts Discussed in Thread: SYSBIOS
Hi
CCSv4.2.1
CGT 7.0.4
BIOS 6.30.03.46
XDCTools 3.20.07.86
We have instantiated a 4096 entry LoggerBuf in our system and our .map file shows a huge memory section allocated below.
00810020 _xdc_runtime_LoggerBuf_Instance_State_0_entryArr__A
00810820
_xdc_runtime_LoggerBuf_Instance_State_1_entryArr__A
00830820
_xdc_runtime_LoggerBuf_Instance_State_2_entryArr__A
It seems to be allocating 0x2000 bytes (128k Bytes) for whatever LoggerBuf Instance State-1 is. Any ideas on how we can reduce state 1 size?
(or maybe 1 entry in the logger buffer is 128k/4k = 32 bytes? - in which case I simply have to set instLoggerBuf0Params0.numEntries smaller).
Also
- The ti.sysbios.rta.Agent configureSystemLog and configureLoadLog are set to false.
- All diagnostics in xdc.runtime.Defaults are set to ALWAYS_OFF and the logger is set to null.
Cheers