Part Number: TMS320DM8148
Hi.
I stream from AXIS camera in H264 format, receive and decode with DM8148. Video data decoding is processed via OpenMax.
At this time, OpenMax returns an error event.
OMX_EventError 0x8000100b
I checked OMX_Core.h
OMX_ERRORTYPE
OMX_ErrorStreamCorrupt "Stream is found to be corrupt"
It was written as above.
Is there a compatibility between the camera and the HW decoder?
Do you have experience decoding with AXIS cameras?
CPU DM8148
SDK EZSDK v5.05.02.00
HDVICP2 H.264 Dec v2.00.00.07
CAM AXIS M1125-E
Operating environment
| CAM | ---- STREAMING ------> | DM8148 |
(H.264)
Regards,
Hideki