Hi,
I am getting an error when I try to start a debug session. Target is a TMDXIDK5718,
the code was simple hello word example(only printf function). i tried as below link manual as 9.9.9 DSP C66 section
i got error like "break at the address "0x800000" with no debug information, or outside of the program code" when without doing step 9(In order to wake up the DSP1 core from A15, Go to Menu option Scripts->AM572x_Multicore_Initialization->DSP1SSClkEnable_API) it is working.
my doubt is
1. i enabled c66xx[c6000] while creating new project in this case its work on DSP CORE?
2. how to fix this error?
thanks and regards
Chandana