Other Parts Discussed in Thread: AM5729
Hi,
I have a question about memory map of DDR.
DDR start address is 0x80000000 and kernel image is loaded at 0x82000000 in boot process.
Can I change the load address to any address with the DDR space?
I can't information of DDR memory map of boot process in the AM571x Linux SDK as below.
+add
Please answer.
Can I change the load address to any address with the DDR space?
I found below declaration in ti_armv7_common.h
#define CONFIG_SYS_LOAD_ADDR 0x82000000
#define DEFAULT_LINUX_BOOT_ENV \
"loadaddr=0x82000000\0" \
"kernel_addr_r=0x82000000\0" \
"fdtaddr=0x88000000\0" \
"fdt_addr_r=0x88000000\0" \
"rdaddr=0x88080000\0" \
"ramdisk_addr_r=0x88080000\0" \
"scriptaddr=0x80000000\0" \
"pxefile_addr_r=0x80100000\0" \
"bootm_size=0x10000000\0" \
"boot_fdt=try\0"
Best regards.