Part Number: 66AK2G12
Hi,
Our design is supposeed to use 66AK as not only rootcomplex but also endpoint of PCIe.
According to the 66AK2Gx Schematic Checklist, it says "If the PCIE subsystem is connected as an endpoint, it is always best to connect the reference clock
provided by the root complex. If the root complex provides a spread-spectrum reference clock, the
PCIE subsystem may not connect if a separate clock is connected to the PCIE_CLK."
This means " the common Clock architecture" is recommended.
On the other hand, generally speaking, te Separate Clock architecture for 5.0 Gb/S(Gen 2) is also covered.

As for 66Ak, If 5.0 Gb/S(Gen 2) is selected, is it possible to adopt the Separate Clock architecture?
【the Separate Clock architecture】
66AK_1 ------(PCIe)-----> 66AK_2
↑ ↑
refclk_1 refclk_2
【 the common Clock architecture】
66AK_1 ------(PCIe)-----> 66AK_2
↑ ↑
refclk_1 ---------------------------↑
Thanks.