Other Parts Discussed in Thread: OMAP-L138, OMAPL138
My system specs:
Target: C674x core on Zoom OMAP-L138 eXperimenter kit
OS: Microsoft Windows XP Professional w/ Service Pack 3
Code Composer Studio Version: 4.2.1.00004
DSP/BIOS Version: 5.41.07.24
Code Generation tools: TI v7.0.3
NDK version: 2.0 w/ OMAPL138 NSP version 01.00.00.01
Description of Problem:
I am trying to run the HelloWorld NDK example on my development board. I ported the example project into CCS4 and was able to build it with no errors or warnings. When I run the example project, the console window spits out the following:
"TCP/IP Stack 'Hello World!' Application
Using default MAC address
Using MAC Address: 00-08-ee-03-14-6d"
The application never returns an IP address. I have tried pinging and running the winapp program to try and communicate with the C674x core, but I get nothing. I configured the code to use DHCP as well as a static IP address resulting in the same problem. My guess is that the Ethernet PHY is not being initialized properly. I read in an online manual that the "Ethernet jack located on the application baseboard is to only be used with the MII PHY; whereas the Ethernet jack located on the UI board is to be used only with the RMII PHY. " I do not know if this affects me or not.
Please help,
Conrad