Hello all,
I'm following the HW user guide for my board, appendix 8, section 8.1 AM335x ICEv2 Flash Erase because I want to boot my board from the micro SD card.
This section references "File:Isdk spi flasher.zip" which is nowhere to be found. I've installed the CCS 10.1.1 on my windows machine, and also the ti-processor-sdk-linux-am335x-evm-06.03.00.106-Linux-x86-Install.bin on my Linux machine.
I thought that this flasher would be included with the processor SDK, but I can't find it. Could someone assist me with this?
Thanks!